2005-07-19 11:35 PM
2005-07-19 11:35 PM
Hi I'am trying to run the timer3 on the STR710-EVAL board as
TIM_PWMOModeConfig ( TIM3, 0x012b, TIM_HIGH, 0x012b, TIM_LOW ); But i not receive on pin 73/ P1.2 the clk. :-( When i try to run Timer1,or Timer2 it work and i receive on pins P1.7 and P0.13 clk. below a code that i use: int main(void) { #ifdef DEBUG debug(); #endif /* Configure FCLK = RCLK */ RCCU_FCLKConfig ( RCCU_DEFAULT ); // Disable clock division by 2 RCCU_Div2Config(ENABLE); // Gets the Div2 Flag status while (RCCU_Div2Status() == RESET); /* Configure the PLL1 ( * 12 , / 4 ) */ RCCU_PLL1Config (RCCU_PLL1_Mul_12, RCCU_Div_4) ; /* Wait PLL to lock */ while(RCCU_FlagStatus(RCCU_PLL1_LOCK)==RESET); // RCCU_RCLKSourceConfig (RCCU_RCLKClockSource ()); RCCU_RCLKSourceConfig (RCCU_PLL1_Output); RCCU_PCLKConfig(RCCU_DEFAULT); RCCU_MCLKConfig(RCCU_DEFAULT); /*********************************************************/ Freq = RCCU_FrequencyValue ( RCCU_PCLK ); EIC_Init(); GPIO_Config(GPIO1, 0x0002, GPIO_AF_PP); GPIO_WordWrite(GPIO1, 0x0000); /* Initialize the Timer 3 registers to reset values */ TIM_ClockSourceConfig(TIM3, TIM_INTERNAL); TIM_Init ( TIM3 ); EIC_IRQChannelConfig( T3TIMI_IRQChannel, ENABLE ); EIC_IRQChannelPriorityConfig( T3TIMI_IRQChannel , 1); EIC_IRQConfig( ENABLE ); TIM_Init ( TIM3 ); TIM_PrescalerConfig ( TIM3, 0x01 ); TIM_ITConfig ( TIM3, TIM_OCB_IT, ENABLE ); TIM_ITConfig ( TIM3, TIM_OCA_IT, ENABLE ); TIM_PWMOModeConfig ( TIM3, 0x012b, TIM_HIGH, 0x012b, TIM_LOW ); TIM_CounterConfig (TIM3,TIM_START); // Infinite loop while(1); } Thanks for ....