2007-01-07 03:19 PM
2006-03-08 01:49 AM
Hello,
I want to transfer data with a MMC card. What is the maximum speed in Mhz of SPI bus on STR710 chip? Thank you :-)2006-03-08 02:17 AM
I want to know the maximum BSPI bus speed in master mode (in Mhz).
Thanks2006-03-08 02:44 AM
Hi,
Each of the two SPIs allow full duplex, synchronous communications with external devices, master or slave communication at up to 5.5Mb/s in Master mode and 4 Mb/s in Slave mode. Hich :-P2006-03-08 02:58 AM
Thank you very much, but I want to know the max speed of BSPI bus in Mhz.
-> APB1 /6 in master mode = X Mhz ?2007-01-05 02:57 AM
Quote:
On 08-03-2006 at 16:14, Anonymous wrote: Hi, Each of the two SPIs allow full duplex, synchronous communications with external devices, master or slave communication at up to 5.5Mb/s in Master mode and 4 Mb/s in Slave mode. Hich :-P I would to have a little precision : is 4 Mb/s the maximum speed in Slave mode? Is'n it 4.096MHz ? Thanks for reply, Regards,2007-01-07 03:19 PM
It looks like 4.096 mhz is the clock frequency. Did I say the clock frequency. The STR should be running at a higher speed using the PPL. Read the manual on the OSC, PPL and SPI.