2024-09-07 03:56 AM
Hello,
we are interested in high side switches particularly VND7030AJ.
Based on the information provided, it seems like there are discrepancies between the table data and the plots in the VND7030AJ Datasheet.
1) On page 10, Table 7 states that the maximum input low-level voltage is 0.9V and the minimum input high-level voltage is 2.1V. However, in Figure 18, the logic input high-level voltage is around 1.7V, and in Figure 19, the logic input low-level voltage is around 1.3V. This does seem to be a conflict, and it would be helpful to get clarification on these discrepancies.
2) On page 11, Table 9 indicates that the MultiSense clamp voltage in the tens of ISENSE = 1 mA is about -15V. However, in Figure 33 on page 25, the MultiSense clamp voltage is shown to be around -0.7V. This also presents a significant difference that needs to be addressed.
2024-09-07 04:23 AM
I hope they will publish a modified version.