cancel
Showing results for 
Search instead for 
Did you mean: 

M24C02 POR Threshold

yana
Associate

What is the lower limit of the POR threshold value for the M24C02-RMN6TPT?
The datasheet states "lower than the minimum VCC", but we need to know the specific value.
With our hardware, the VCC only goes down to 1.0 V, not 0V.  Therefore, I am inquiring to make sure that Device Reset is working reliably.

4 REPLIES 4
Mike_ST
ST Employee

Hello,

Your device is M24C02-RMN6TPT, so tables 6 and 21 in the datasheet tell that this value is 1.8V:

R = VCC = 1.8 V to 5.5 V

 

Ok, but that's the voltage range for reliable operation. The question here is more about some degree of viability and retention which is likely much lower.

Is there a POR circuit internally that clamps it in reset below 1.8V ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Has POR internally https://www.st.com/resource/en/datasheet/m24c02-r.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
yana
Associate

Hello,

What is the threshold range that its internal POR operates in?

For example (1.8-1.6V) or (1.8V - 1.4V) or .....?