2004-12-08 08:57 PM
2004-12-06 11:14 PM
We are designing our hardware right now and have one question regarding the BSPI pin /SS.
We will use one of the BSPI ports to clock data into and out of a large shift register. For that we will use the SCLK, MISO and MOSI pins (in Master mode). My question is: Can the /SS then pin be used as a general output? Or will the ARM make it go low when I'm tranceiving data in Master mode? In the refernce manual page 266 it says:2004-12-07 04:47 AM
Hi Yxan,
It's not possible to use the SSN pin as you described it in your message, the STR71x reference manual note that the the /SS pin must be asserted high on the master mode ,and this in order to avoid to have two master device at the same time. I hope that can help you Best Regards. Hich ;-)2004-12-07 08:59 PM
Hi Hich,
Ok, I see that it says that the /SS pin must be asserted high. But why???You say: ''to make sure there isn't more than one master at the same time'' But I still dont understand, I slave mode the /SS pin is used as an input - OK I master mode the pin is not used but it must kept in high state. WHY????? :-o Sorry for not just accepting it, I want to know why the pin cannot be used. Yxan2004-12-08 08:23 PM
Hi Yxan,
In master mode this pin is used to detect that more than one device has acted as a Master simultaneously on the BSPI bus. The BSPI, configured as a master, will generate a Bus Error condition. This error is defined as a condition where the Slave Select line goes active low when the module is configured as a Master. This indicates contention in that more than one node on the BSPI bus is attempting to function as a Master. Best Regards. HICH :-P2004-12-08 08:57 PM
OK, now I understand.
Unfortunally this means one pin less to play around with. Thanx for the clarification /Yxan/