hi, im benarjee working as a Asst.manager .since two months im working on STR912 bootloader implementation for loading the code via the pen drive .
can anyone help me out how to solve it?
can anyone help me out how to solve it?
How to use the "Ultrasound Pulser Waveform Demo" with STEVAL_IME013V1 EVB to generate waveform in 40KHz ?
simulation over temperature range +25°C to +107°C of SM6T10A, PSPICE model downloaded from STMicro site, is far from real behaviour. At +25°C, VBR = 10.12V for IR = 1 mA, at +107°C, VBR = 244.8µV for the same current. With alphaT = 7.3 10e-4/°C (see ...
Hi,I am trying to develop a switch that can turn on various loads in motorsports vehicles. I made a prototype using the VN7003ALH. The first thing I tried to switch on was a cooling fan. Which specified a 20 amp load max (obviously on start up it wil...
We are still buying M68AW128ML70ND6 (SRAM) from brokers. Its datasheet does not specify any RoHS status. We would like to know if the part was ever manufactured as ROHS compliant ? If so, from which date code was the part RoHS compliant ? Thanks in a...
On the SPWF01 module TLS anonymous negotiation was possible (ie no client copy of the server certificate required). Is this possible on the SPWF04? The documentation alludes to anonymous negotiation in AN4963 Section 1.1 - TLS sub Protocols on page ...
Hello,I am going to adopt the STR71x(HDLC) on our system.But I can't find any document and sample code for the HDLC of the STR71x.Could you help me to find those sources?Thanks
Posted on September 09, 2017 at 10:44Hello,I have a lot of CR95HF for a project that could read NFC Tags of a medical equipment and send this via bluetooth to a smartwatch.I works but i would have now the Pulse W7001 NFC antenna on the CR95HF Chip a...
Hi,I designed a board integrating a High Side L9733.I try to communicate with the switch through SPI but I miss some informations.1- Can you confirm that we can use a 1.8V SoC as master?I fixed VDO to 1.8V. I didn't find nominal range for VDO. (only ...
I'm trying to get a hold of 500 units of VNQ7140AJTR and I've been unable to find any in stock at any distributor. I placed an order with Digikey about a month ago and it has been on back order since then. They are not able to give me an expected del...