Hi , GuysDoes anyone have BSDL file for this one ? GM1601-LF-CFI am appreciated anyone's helpBest all ,
Hi all. I'm about to start a project where we just measure the voltage and current of a single phase 220V 50Hz line. We need all the usual values (P, Q, S, cos phi, etc) using a CT and a standard transformer for the voltage. We also don't care that m...
Hi sir,As per our application, we need to enable and disable the power supply IC enable pin. So we are using Flip flop based toggle function. so we are connect 12V rail directly (before voltage regulator).So as per ISO standard, our application shou...
It seems that the reference SPBT2632C2A.AT2 (Bluetooth V3.0, Class2) is unavailable.Therefore, we would like to know about a available compatible reference, both hardware and firmware.Could you help me with this issue?
We have material that have material as top marking 456R8 under MPN MT24256-BRMN6