2018-06-14 5:41 AM
Hi I am designing a Locomotive application with my customer, we have selected part# SPC560P54L3BEABY for 3.3V application. Now the end customer demands 5V application too. I learnt that the same series doesn't have a 5V part.
Our code is developed on SPC560P54L3BEABY , will the same code will work on SPC560P60L3CEFAR, or do we have to change our code. I see the part are pin to pin compatible and the only difference is the Flash Size.
2018-06-15 7:04 AM
hello Manas ,
i will check with our designer
Best regards
Erwan
2018-06-18 2:41 AM
Hello Manas ,
SPC560P54L3BEABY is 768K flash size in LQF100
SPC560P60L3CEFAR is 1M Flash Size in LQFP100
It is PIN Compatible you can use the same code in SPC5Studio Application.
Otherwise , just change your linker file.
About voltage,
You can find in the chapter 3.4 some useful informations about Recommended operating conditions.
Best regards
Erwan