cancel
Showing results for 
Search instead for 
Did you mean: 

M41T81S – How to handle RTC Oscillator Stop/Fail Bits

Central SUPPORT
Senior II

In Datasheet Table 5 it says that the Oscillator Fail bit OF (Clock register: bit 2 of address 0Fh) starts at “1�? after initial power-up. So, in this case (or whenever when I find OF bit at “1�?) I will have to restart the oscillator by pulsing Oscillator Stop bit ST (Clock register: bit 7 of address 01h) resp, write “1�?, then “0�?.

Then it says that I have to wait another 4 seconds before clearing OF bit. Is this a must?

0690X00000895WvQAI.png

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Central SUPPORT
Senior II

Technically, you can clear the OF bit without waiting 4 sec, but it can happen that system will set it again if the oscillator is not stable yet.

Refer to AN3060 “Applications guide for serial real-time clocks (RTCs)�?, chapter 6.1 for more details.

View solution in original post

1 REPLY 1
Central SUPPORT
Senior II

Technically, you can clear the OF bit without waiting 4 sec, but it can happen that system will set it again if the oscillator is not stable yet.

Refer to AN3060 “Applications guide for serial real-time clocks (RTCs)�?, chapter 6.1 for more details.