cancel
Showing results for 
Search instead for 
Did you mean: 

CUT information for SPC574K7x

eantonioli
Associate II

What does it mean CUT?

I suppose is a CPU identification tag, but I'm not sure.

I developing a project with SPC5 studio V.6.0, but I don't understand which file I must include in my project between spc574k_cut24.h and spc574k.h.

I see there are some example for CUT 2.3 and CUT 2.4 but I don't known the differences.

Can anybody help me, please?

Thank you very much.

Best regards

E.

1 ACCEPTED SOLUTION

Accepted Solutions
Giuseppe DI-GIORE
ST Employee

Hello,

the register SIUL_MIDR1 contains the information you are looking for.

Regards,

Giuseppe

View solution in original post

3 REPLIES 3
Erwan YVIN
ST Employee

Hello ,

CUT is an hardware version. (2.4 is more recent than 2.3)

A different hardware can impact the include file (registry file).

a simple diff , you can see the difference in term of IPs or registry.

normally , some basic example should work on the 2 cuts.

Best regards

Erwan

eantonioli
Associate II

Hello,

thank yuo very much for the quick reply.

But where can I found in the ST documentation, what CUT can I use with my devices? (now I'm developing on SPC574K72E5).

For example, in SPC5Studio I can find two CAN examples, one for CUT 2.3 an one for CUT 2.4. Which example can I use for the SPC574K72E5?

Best regards

E.

Giuseppe DI-GIORE
ST Employee

Hello,

the register SIUL_MIDR1 contains the information you are looking for.

Regards,

Giuseppe