Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Hello Dear ST Community I am Salih, Electrical Electronics Engineer and Software Developer. I am developing software for functional security in the automotive industry in a company.

For this reason, we need an Eval Board that meets the requirements I will list below. I request your suggestion equipment.Thank you,Requirements;There must be a debugger for the uC on the development board.uC must have Ethernet, FlexRay, USB, SDHC, C...

MKara.7 by Associate
  • 317 Views
  • 1 replies
  • 0 kudos

Resolved! I want to connect to the SPC584B-DIS with SPC5Studio, however I always get the following error when trying to validate a project on the board: "LOAD ERROR: STM32 - no connected board(s), invalid firmware or the board should be re-started"

Hello,I am currently trying to run a Machine Learning application on the SPC584B-DIS MCU. I used SPC5Studio with the AI plugin to create the project and it compiled without an error. The board is connected to the PC by USB cable. When I try to valida...

FDado.1 by Associate
  • 277 Views
  • 1 replies
  • 1 kudos

Resolved! Frozen ADC Bits in Debug Mode

Hello,How can I watch the values of global or static variables for ADC Module. When I add the variables which keeps data to the watch table, I dont see what's going on. They don't change. ( Also I wanna learn this for Timer and other Modules)

Msert.1 by Associate III
  • 517 Views
  • 3 replies
  • 0 kudos

How to configure HTTP/FTP example

Hello folks,I'm playing around with the SPC58 discovery kit and trying to setup the HTTP/FTP worked example. It doesn't appear to me that out of the box that FTP nor HTTP code on the target runs correctly. I can ping the discovery kit, so clearly the...

RSmit.12 by Associate II
  • 331 Views
  • 1 replies
  • 0 kudos

Resolved! SPC574S Dead-Time

Hello,1) Where is the reference manual of SPC574S-DISP. I could not find it. What will I take reference for programming?2) I want to create dead time on my PWM signals. I know how to create a PWM signal. How to add dead time to PWM signals.Regards,

Msert.1 by Associate III
  • 579 Views
  • 3 replies
  • 0 kudos

SPC58 Network RLA/DHCP Issue

I had a functioning TCP/IP application I am trialing on the SPC58EC-DISP discovery board using DHCP. SPC5Studio pulled updates and is not forcing me to migrate to the latest RLA (1.8.2.20200908161300) which breaks some network code -- this was fixed....

VMiki.1 by Associate II
  • 644 Views
  • 5 replies
  • 0 kudos