Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

I am configuring the flexray controller.After setting the parameters, a RUN command is given which changes the POC_state from POC:ready to POC:startup. But further change of state to POC:normalactive is not observed.

The FlexRay cluster I have here consist of 2 FlexRay cold-start nodes and the third node, spc58ec mcu non-cold start node. Can anybody suggest what can go wrong ?

RSeba.2 by Associate III
  • 2112 Views
  • 4 replies
  • 0 kudos

Resolved! FreeRTOSConfig.h file patching mode

I want to trace ContextSwitchIn and ContextSwitchOut events. I defined two functions for this. #define traceTASK_SWITCHED_OUT() getTASK_SWITCHED_OUT_EVENT(pxCurrentTCB) #define traceTASK_SWITCHED_IN() getTASK_SWITCHED_IN_EVENT(pxCurrentTCB)I put the ...

0693W00000YAanZQAT.png
sonerb by Associate II
  • 1498 Views
  • 2 replies
  • 0 kudos

Resolved! Failed write the IIC register ICBR of SPC584C70E3FMC

After IIC module is initialized, when I prepared the data and to write the IBCR register to send it, after the register is written with the value 0x70(master mode, tx mode, interrupt enable and generate START condition), the value read from the IBCR ...

0693W00000YAPjbQAH.png 0693W00000YAPjlQAH.png
JJaso.1 by Associate
  • 1628 Views
  • 2 replies
  • 0 kudos

Resolved! Calculate crc in spc5studio and SPC58ECxxxx MCUs

I am using spc5studio and SPC58EC80E1.i import crc sample from application library.i set CRC Settings at low level Drivers component RLA - CRC-32, Polymonial seed 0x4c11db7, reset = 0xFFFFFFFFand firmware code​----------------------------------------...

PLEE.2 by Associate II
  • 1697 Views
  • 3 replies
  • 0 kudos

Resolved! WINDRIVER compiler

We use WINDRIVER compiler to develop software on ST chip. Can you provide the example mentioned in AN5171 file?SPC560Dxx_RLA PIT WINDRIVER.zip

ligbt.1 by Associate
  • 1256 Views
  • 2 replies
  • 1 kudos