Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC58: UART Tx DTF_TFF is not working

Hello, I was implementing UART in interrupt mode on SPC58 (using SPC5 stduio sample code) and encountered an issue where DTF_TFF does not occur during operation. For example, when I request the transmission of 23 bytes, DTF_TFF randomly does not occu...

SKang.9 by Associate
  • 874 Views
  • 0 replies
  • 0 kudos

SPC58EC HALT0 mode related query

Hello, I have a question regarding the HALT0 mode. Is it possible for the FlexRay core to read the data from memory while CPU is on halt (in HALT0 mode core clock is stopped)?In general, is there some kind of setting in SPC58EC mcu where system memor...

RSeba.2 by Associate III
  • 796 Views
  • 0 replies
  • 0 kudos

Resolved! board.c generation

HiI have an imported project and I would like to modificy the GPIO configuration inside board.cI saw board.c is a file generated from pinMapEditor configuration but is I open the project and the PinMapEditor page I'm not able to modify anything becau...

Resolved! SPC58

We are using SPC58NH-disp.We are developing a software that we want to print the data we receive over CAN-FD to the screen with TCP.We are using a Simple TCP Echo Server Demo for TCP.Data flow takes place indefinitely and in indefinite numbers.But su...

SPC58NH by Associate II
  • 2180 Views
  • 4 replies
  • 0 kudos

SPC564: Sample code with external Memory

Hi,I am trying to access external SRAM with the SPC564A80, but I always get a machine check exception.I suspect an error in the initialisation, but cannot find a cause.I am urgently looking for sample code or other support to realise the memory acces...

Mp_Esp by Associate
  • 706 Views
  • 0 replies
  • 0 kudos

Resolved! SPC5 Controller is Heating and not connecting with debugger.

Hi, We are using an SPC5 microcontroller for a motor controller application. All of a sudden, we weren't able to connect with our motor controller board, which runs on the SPC5 controller, and we also found that it was getting heated up to 36 °C. and...

SV.9 by Associate II
  • 1438 Views
  • 2 replies
  • 0 kudos