Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

spc58 jtag/Nexus

I through Nexus to read/write memory.Is the response correct?The steps to enter Nexus from jtag are as follows:1. TDI: Shift-IR(0x01) Shift-DR(0x00000000) TDO: 0x11140041it confirms the jtag id is correct2. TDI: Shift-IR(0x2A)it through jtag to enabl...

and_w_0-1732692150611.png
and_w by Associate
  • 642 Views
  • 0 replies
  • 0 kudos

spc582b register

Is the  base address  of Flash user registers  0xF7FE0000. In rm0403,I don't seem to have found any other relevant addresses。 

and_w_0-1732671029472.png
and_w by Associate
  • 542 Views
  • 0 replies
  • 0 kudos

MCU SPC58

Hi anyone could help me how to read this ecu infineon micro using bootmode?oR HOW TO READ THIS FLASH MEMORY

image_67511809 (1).JPG image_67239681.JPG
rashed420 by Associate II
  • 1868 Views
  • 3 replies
  • 0 kudos

Resolved! SPC5 Studio

Hello, I am Erdem.I am an R&D engineer at Devimsel Elektronik. I will use the SPC560P processor on my own PCB board. For this I need instructions for using SPC5 studio. How do I make configurations such as pin and clock tree? Can I get an instruction...

Eakso.1 by Associate II
  • 4131 Views
  • 6 replies
  • 1 kudos

Resolved! EV-VN9D30Q100F for SPC582B-DIS or SPC58EC-DIS GUI firmware

Hi,i need some help for the EV-VN9D30Q100F. It says there is a dedicated Software for the SPC582B-DIS or /EV but i can't find it nowhere. The board connects to the GUI (STSW-EV-M09SPI), so far so good, but without the firmware on the MCU, i can't tes...

PNeub.2 by Associate II
  • 1002 Views
  • 1 replies
  • 1 kudos

Resolved! SPC560P50L5 CAN Module doesn't work successfully

Hello everyone.Because I need to test a newly purchased SPC560-DISP, I tested several commonly used modulesAnd these is my test devices:Devices Used:MCU: SPC560P-DISPCAN: Kvaser Leaf LightV2I conducted tests on several commonly used modules:PITEIRQPW...

Louie33 by Associate II
  • 1232 Views
  • 3 replies
  • 2 kudos

Resolved! searching for datasheet SPC58VX829348

i have looked everywhere and cant find the datasheet for this mcu, we get alot of this becouse we are in the business of reusing dismantled ev car batteries and as much components as possible.with this we are building Energy storages for grid service...

sebbeben by Associate
  • 1990 Views
  • 2 replies
  • 2 kudos

SPC58EC80E5- ISOSPI Launching error

Dear all,I am using AEK-POW-BMS63ENA connected via AEK-COM-ISOSPI module to  AEK-MCU-C4MLIT1 for measuring the voltage, current and temperature of 14 lithium ion battery cells connected in series.after running the demo provided in AutoDevKitStudio, (...

error.JPG signal-2024-11-13-223541_002.jpeg