cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DW12 consumption in fifo mode

laesser
Associate II

Hello, 

I'm using the LIS2DW12 on my own board.

Consumption seems a little high to me. In the datasheet I found a value around 5.5µA and I obtained rather 45µA.The configuration is as follows:
- ODR 50Hz
- FIFO in continious mode with INT1 enabled

- Full-scale 4g

- 14 bits resolution in LP2.

I did not find any information regarding consumption in FIFO mode. Can you give me some information?

Thanks

0 REPLIES 0