Skip to main content
Snara.21
Senior
February 4, 2022
Solved

Power consumption analysis for SensorTile.Box

  • February 4, 2022
  • 1 reply
  • 927 views

I want to calculate the Power consumption in Sensortile.Box . Is there is any document or tool for analysing the present consumption rate and the areas to be optimised. I am planning to develop my own hardware.

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @Snara.2​ ,

    The power consumption of a board depends upon the firmware that is running. This affects the current that flows from the rechargeable Lithium-ion battery (3.6V).

    SensorTile.box firmware perform an estimation of the battery level (that is displayed in the STBLE app homepage), but doesn't.

    Since you are planning to develop your own hardware, my suggestion is that you should monitor the consumption on the general Vdd line through a shunt resistor that can be connected to the microcontroller ADC, and that gives you a measure of the real time current consumption.

    You might take inspiration from the STEVAL-MKI109V3 schematic, that is a bit complex but very precise (p.4), but probably a simple shunt resistor could be enough.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

    -Eleon

    1 reply

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    February 4, 2022

    Hi @Snara.2​ ,

    The power consumption of a board depends upon the firmware that is running. This affects the current that flows from the rechargeable Lithium-ion battery (3.6V).

    SensorTile.box firmware perform an estimation of the battery level (that is displayed in the STBLE app homepage), but doesn't.

    Since you are planning to develop your own hardware, my suggestion is that you should monitor the consumption on the general Vdd line through a shunt resistor that can be connected to the microcontroller ADC, and that gives you a measure of the real time current consumption.

    You might take inspiration from the STEVAL-MKI109V3 schematic, that is a bit complex but very precise (p.4), but probably a simple shunt resistor could be enough.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

    -Eleon