Skip to main content
reefwing
Associate II
October 12, 2024
Solved

Calculating THRESH1 for the FSM and ISM330BX accelerometer

  • October 12, 2024
  • 2 replies
  • 1001 views

I'm doing a 4D orientation detection FSM on the ISM330BX. There is no example for this IMU so I'm following the examples for some of the other IMUs. That is fine and the code works, but what I can't work out is how to calculate the THRESH1 value and get it to agree with the value displayed in MEMS-Studio.

As shown in the attached screenshot, 0x3A66 (14950 in decimal) is shown as 0.8 g in MEMS-Studio for the ISM330BX, but if I work it out:
Value in g = 14950 x 0.000061 g/LSB = 0.913 g

Any ideas on what I am misunderstanding?

It doesn't really matter from a FSM perspective whether THRESH1 = 0.8 or 0.91 g but still...

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @reefwing ,

FSM thresholds are stored in registers in half-precision floating-point format, so 0x3A66 does not actually represents 14590, but 0.8.
Moreover, FSM threshold values are independent from full scale, and what is stored in registers is directly the value in g.
Therefore, 0x3A66 represents a threshold of 0.8 g independently from the selected full scale.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
October 15, 2024

Hi @reefwing ,

FSM thresholds are stored in registers in half-precision floating-point format, so 0x3A66 does not actually represents 14590, but 0.8.
Moreover, FSM threshold values are independent from full scale, and what is stored in registers is directly the value in g.
Therefore, 0x3A66 represents a threshold of 0.8 g independently from the selected full scale.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
reefwing
reefwingAuthor
Associate II
October 15, 2024

Hi @Federica,

Thank you very much, it was driving me crazy that I couldn't work it out!