MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

community.st.com

Posted on February 17, 2017 at 11:04ST politics about VL53l0X Hy ST,in a customers project I deal with the VL53l0X quite a bit, we have a nice prototype up and running and are about to decide if we want to start designing a series device.Ever once i...

harald by Associate III
  • 671 Views
  • 3 replies
  • 0 kudos

Interpretation of output of LSM6DS33

Posted on March 01, 2017 at 08:30Hi,In the 'Examples of output data' section of the LSM6DS33 application note AN4682, there are tables showing examples of the output register values and the corresponding acceleration and angular rate values for a gi...

prachi by Associate
  • 850 Views
  • 1 replies
  • 0 kudos

LSM9DS1 SPI not working

Posted on February 26, 2017 at 23:32Hello.I´m having problems on SPI reading WHO_AM_I register of a LSM9DS1 mounted on STEVAL-MKI159V1 : the correct answer is 0x68 but very often I got 0x28. The suspect that the level of bit 6 was not correctly set...

LIS2DH12: do I need a different accelerometer?

Posted on February 28, 2017 at 00:33Hey,   In my application there is a lot of high frequency vibration that I am not interested in. The goal is to detect acceleration along a single axis that lasts 200ms or longer, but is generally between 1/2 and ...

How to detect click/double click with LSM9DS1

Posted on February 27, 2017 at 08:17Hello everyone,In the data sheet of LSM9DS1, it is stated in the first page that the device supports: Position and motion detection functionsClick/double-click recognitionHowever I cannot find anywhere in the...

Implementing Complementary Filter

Posted on February 24, 2017 at 20:11Hello everyone,To make this quick, I'm hoping to find any guidance on a particular issue we're having.We've developed a prototype wearable using ST's accel/gyro/magneto module. However we're trying to reduce the e...

LSM6DSL on IKS01A2 board won't put gyro data into the FIFO

Posted on February 23, 2017 at 08:04Hi all,I'm playing with the LSM6DSL sensor on the IKS01A2 board.I'm trying to use the FIFO to record and buffer accelerometer and gyro data.The accelerometer works fine and reading the gyro registers directly give...

Half sensitivity of one VL53L0X

Posted on November 07, 2016 at 11:56Hy,for a proof of concept I created five identical devices, each having 3 VL53L0X, so I have an overall of 15 VL53L0X that are mounted (behind an acrylic glass shade) and connected (via 2.8V, I2C) identically. Dur...

harald by Associate III
  • 552 Views
  • 2 replies
  • 0 kudos