MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Ultra-low power IMU for step counting

I need to develop a low-power embedded device with pedometer functionality. I'm looking at the LIS3DH because of it's low power, but there's no built-in pedometer application. I've also looked at the LSM6DSL, as it has built-in pedometer support, but...

LPS22DF for new design

Hello,Please the pressure sensor LPS22DF is it recommanded for a new design ?Thank you

ljm by Associate III
  • 761 Views
  • 1 replies
  • 0 kudos

Issue with Wrist Tilt Direction Detection on LSM6DS3TR-C

Issue with Wrist Tilt Direction Detection on LSM6DS3TR-CHardware & Software Details:- Sensor: LSM6DS3TR-C- Platform: Arduino- Interface: I2CProblem Statement:We are working on detecting wrist tilt using the LSM6DS3TR-C sensor. While the tilt detectio...

Screenshot 2025-02-24 112515.png Screenshot 2025-02-24 121811.png Screenshot 2025-02-24 121759.png Screenshot 2025-02-24 115620.png

Inactivity Mode for the lsm6dsv16x IMU

Hello there,  Are there any examples on how to use the inactivity feature of the lsm6dsv16x?I checked the github and I only see for waking up, but not the other way around. My goal is to set a device to sleep once there is no motion from imu. meaning...

ACand.3 by Associate III
  • 1135 Views
  • 1 replies
  • 0 kudos

Resolved! Trying to understand/use MotionGT library

Hello,I'm trying to calibrate the gyroscope of LSM6DSO MEMS but I don't really understand what describe the quality parameter in the MGT_state_t structure. I didn't find any information about it in the datasheet. Could you explain it to me ?I succeed...

AKE1_0-1740048512741.png AKE1_1-1740048710872.png
AKE1 by Associate II
  • 1560 Views
  • 3 replies
  • 0 kudos

Resolved! LPS28DFW one shot bit cleared before sample is ready?

Hi, I'm trying to use the LPS28DFW in one shot mode and there seems to be a discrepancy between the devices functionality and the application note.From an5758 section 3.2 - one shot mode: "One-shot mode has to be executed while the device is in power...