MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using INT2 on LIS3DSH for DRDY signal

Hi,I'm using a STM32F4 board which has a LIS3DSH. This board has PE0 connected to the INT1 of the LIS3DSH and PA0 connected to the user Button B1. Due to this, I won't be able to use interrupts to sample and interrupt for button press. I'm trying to...

GTS.1 by Associate III
  • 1695 Views
  • 3 replies
  • 0 kudos

Question from Predictive Maintenance Webinar 29th of April: Question on encryption hardware solutions and importance of secure TRNGs and QRNGs, see details section:

1) What are the current encryption hardware solutions based on which are used for designing PdM and CM applications? 2) How important is the use of cryptographically secure TRNGs or QRNGs for industrial IoT applications and what are the current hardw...

Question from Predictive Maintenance Webinar 29th of April: Can the STEVAL-BFA001V2B be interfaced with P-NUCLEO-IOM01M1?

Can the STEVAL-BFA001V2B be interfaced with P-NUCLEO-IOM01M1: STM32 Nucleo pack for IO-Link master with IO-Link v1.1 PHY and stack ? i choosed this second board because at the moment the STEVAL-IDP004V2 is not available at the moment from distitribut...

VL53L1X Low Temperature Performance

We using the VL53L1X in an application where it will be mounted in a manner that's protected from sunlight, but exposed to cold ambient temperatures - -40°C and possibly lower. The VL53L1X datasheet has a lower operational temperature limit of -20°C...

DAmer.1 by Associate
  • 964 Views
  • 1 replies
  • 0 kudos

STEVAL-STWINKT1, any WiFi tutorials?

Is there any tutorials/AN for using the WiFi connectivity on the STWINKT1 board? What dashboard can i use to display sensor readings?

TResell by Associate II
  • 1096 Views
  • 1 replies
  • 0 kudos

Resolved! Get factory settings/ firmware of the STEVAL-BCN002V1B

Hello,I have a question to the STEVAL-BCN002V1B. I try some BLE-Examples and flash the bord with some firmware example from the SDK. Now I can't pair the board with my mobile phone ST APP. Which firmware do I have to use to get the default factory s...

MMaie.1 by Associate II
  • 1652 Views
  • 2 replies
  • 0 kudos