MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I easily combine the LSM6DS0 and the NUCLEO-L496-ZG?

In our current project, we chose a NUCLEO-L496 ZG as the core of our prototypes hardware. Now I am interested in combining the board with two fitting inertial measurement units. I think that the LSM6DS0 would be a good choice. How would you combine t...

MAlte.1 by Associate
  • 794 Views
  • 1 replies
  • 0 kudos

Hi, our designers are incorporating pressure sensor LPS22HH in to a product that requires post-assembly washing, prior to conformal coating. I can find very little information in the product literature relating to washing. Is this product washable?

Our standard washing process uses Vigon A201 chemistry at a 15% concentration in D.I. water. The washing solution is heated to 65 deg. C.Can anyone advise if this part is robust enough to withstand this process, perhaps if it has a post-washing bakin...

PBart.2 by Associate
  • 1752 Views
  • 2 replies
  • 0 kudos

ST Pedestrian Dead Reckoning Algorithm

Where can I find more info on ST Pedestrian Dead Reckoning Algorithm , I see a presentation from a past showcase, but nothing else. Anyone knows where I can get it, or who can I contact ?

EGarc.2 by Associate
  • 1799 Views
  • 2 replies
  • 0 kudos

I do not set the low power mode of the LIS3DH sensor properly.

I am using the ST LIS3DH sensor, and would like to try the low power operation mode, but the results I see on the display are not what I expected, since at rest, instead of seeing values of + -1g, I see values of + -3g, with a full scale of 2g.And I ...

EEstr.1 by Associate II
  • 3409 Views
  • 8 replies
  • 0 kudos

Resolved! Hello, I'm currently testing the IIS3DWB accelerometer. The Datasheet says that the Timestamp tick resolution ist 25 us. All my measurements show, that the real resolution is 12.5 us. Is this correct?

This actually makes sense because the ODR is 26,667 kHz which means that between two samples are 37.5 us this would make three 12.5 us ticks. 25 us wouldn't make much sense.

MNoll.2 by Associate II
  • 2096 Views
  • 4 replies
  • 0 kudos

Question regarding implementation of LIS3DSH Standard C library.

Hi,I was taking a look at the STMems Standard C Library for the LIS3DSH. The implementation of the function lis3dsh_status_get looks a bit weird as there are 2 calls to the lis3dsh_write_reg functions.int32_t lis3dsh_status_get(stmdev_ctx_t *ctx, lis...

GTS.1 by Associate III
  • 2013 Views
  • 4 replies
  • 1 kudos