MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

100-3000 psi pressure sensor to long distance WIFI.

I want to build a communications device that looks at 100-3000 psi pressures in my chemical plant and transmits the data to a receiver and GUI in the control room on a dedicated workstation. I am thinking it will take a .5-4.5 VDC pressure transducer...

TMCGE.1 by Associate
  • 1806 Views
  • 3 replies
  • 0 kudos

I downloaded the Sensortile Gerber files provided on the website, there are only three layers in the folder. I assume there whould be a 4th, is it possible to have further info about it? Thank you very much

I got the answer through other channels, posting here just in case it can be useful for someone else.Sensortile has 4 layers:   - STLCS01V1.cmp - top layer    - STLCS01V1.sol - bottom layer    - STLCS01V1.l15 - internal layer 1    - STLCS01V1.ly2 - ...

FBuff.1 by Associate
  • 958 Views
  • 1 replies
  • 0 kudos

Where is the source code for Predictive_Maintenance_BLE application.The Predictive_Maintenance_BLE application is part of the FP-IND-PREDMNT1 STM32Cube function pack. It allows developing a sensor node for condition monitoring and pr

I have reviewed the user manual for How to use the STEVAL-STWINKT1 SensorTile Wireless Industrial Node for condition monitoring and predictive maintenance applications. I have the latest CubeMX

Sudhir by Associate III
  • 1161 Views
  • 2 replies
  • 0 kudos

LIS3DSH Wake-up exemple interrupt only once ?

Hello all, I have set up the "Wake-up" example that you propose on page 75 of the technical documentation (see attached picture).My problem is that the interrupt during a movement is executed only once. How can I make sure that an interrupt is genera...

Rgerg.1 by Associate
  • 1213 Views
  • 1 replies
  • 0 kudos

Resolved! Help reading accelerometer on B-L475EIOT01A2C board.

I am new to the STM32 Cube IDE and TRUESTUDIO software. I have followed the step-by-step guide given on the website which allows the user to read the temperature input on the board. However, I am wondering if there is any guidance available for being...

JMerr.1 by Associate II
  • 2355 Views
  • 2 replies
  • 0 kudos

Resolved! SensorTile.box Algobuilder User Button not working

Hi!I am using the SensorTile.box together with Algobuilder. Since 2.6 there is the feature that pressing the user-button triggers data collection.Unfortunately this does not seem to work with SensorTile.box. I am using the Example13_SensorTile.box_SD...

0693W000001pWpqQAE.jpg
DWind.1 by Associate III
  • 1976 Views
  • 2 replies
  • 0 kudos

Internal temperature sensor, on a STM32H7 board

Hello, I want to read the value from the internal temperature sensor, on a STM32H7 board, but it is not very clear in RM0433 which unit should have the TS_DATA (voltage or ADCCounts) and if I should use a conversion factor or not.Could you, please, g...

0693W000001pVDCQA2.png
DPetr.2 by Associate
  • 1775 Views
  • 3 replies
  • 0 kudos

VL53L0X sensor read not working

Hi,I try to read the VL53L0X sensor using the continuous read function. When I try to read the register 0x14 (result range status) + 10, I always get a fix value of 0x1FFF.

VLao.1 by Associate
  • 809 Views
  • 0 replies
  • 0 kudos

Is LSM303AGR DRDY signal mandatory to use Linux 4.14 ST driver?

Hello,We are encountering an issue using magnetometer function of a LSM303AGR.I2C line is OK, we can read WhoAmI register of both accelerometer and magnetometer using low level I2C functions. So we can retrieve accelerometer data without any problem ...

SSERR.11 by Associate II
  • 2991 Views
  • 5 replies
  • 0 kudos

LSM303AGR accelerometer disappointing accuracy

I configured LSM303AGR accelerometerit for high accuracy mode 50Hz and I am reading it at 20 Hz via i2c.The xyz signals are very unstable, and the final angle calculated (see figure) has huge variations. 2 degrees is far from what my expectations for...

0693W000001ceuOQAQ.png
GDemu.1 by Associate
  • 1687 Views
  • 2 replies
  • 0 kudos