MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! will vl53l0x work in outdoors?

I performed all the calibrations indoor and whenever i am testing it in outdoor(both under direct sunlight and opposite) ,it is always detecting some particle without any interference.Do i need to perform calibrations again in outdoor?

ANANTH by Associate
  • 1453 Views
  • 1 replies
  • 0 kudos

Resolved! What is the ZERO offset value of LIS3DH after Factory Calibrated?

HI, After Factory calibration of LIS3DH accelerometer, what are the range of values given by the accelerometer( Selected 12 bit OUTPUT). I am getting 20-30 ADC counts of X axis from accelerometer, where as -1 to 3 counts from Y axis . Why there ...

NMale.1 by Associate III
  • 1576 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DE12 I2C write timeout

My application is very low power, and I need to save power wherever possible. To this end, I do the following:LIS2DE12_WriteReg(LIS2DE12_MEMS_I2C_ADDRESS, 0x20, 0x08);Which basically puts the accelerometer in power down mode. The LIS2DE12_WriteReg ba...

Resolved! lis3mdl connected to lsm6dsox I2C

Hello, support team.In my test board, lis3mdl is connected to lsm6dsox I2C.From above board, I want to read acceleration and gyro at 1667Hz, magnetic at 1kHz.I refer to lsm6dsox_sensor_hub_fifo_lis2mdl.c to implement SW.But It looks like magnetic da...

JPARK.2 by Associate II
  • 2059 Views
  • 2 replies
  • 0 kudos

Resolved! Why LSB register is always giving ZERO in LSM3DH accelerometer?

HI,In LSM3DH accelerometer sensor datasheet given output of accelerometer is 16 bitthey are divided into two 8bit registers. MSB, LSB registers. LSB register is always giving ZERO as output. only MSB register is giving output.Why LSB register is alwa...

NMale.1 by Associate III
  • 2423 Views
  • 3 replies
  • 0 kudos