MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DW12 VDD_IO current way too high!

Hey There, iam using a LIS2DW12 on a STEVAL-MKI179V1 eval board :https://www.st.com/en/evaluation-tools/steval-mki179v1.html#overviewhttps://www.st.com/en/mems-and-sensors/lis2dw12.html#overviewThe Datasheet says that it has 50nA standbycurrent and 1...

MSimo.1 by Associate II
  • 5345 Views
  • 9 replies
  • 0 kudos

Pulsed IR transmitter doubt

 Hello.I had to interface an IR sensor for object detection and distance measurement but I'm using a normal IR transmitter and receiver and there's a lot of interference due to sunlight. So I want to pulse the IR transmitter and subtract the readings...

0693W00000Y9S0hQAF.png

ASM330LHH didn't work in I2C with BLUENRG-LP

Here I used BLUENRG-LP SoC with ​ASM330LHH. We have the same schematic design in steval-IBD11V2A, like the first image. The second one is our schematic design.My I2C configuration init function is like:/** * @brief Configures the I2C interface use...

0693W00000WL0FuQAL.png 0693W00000WL0GTQA1.png
EPeng.1 by Associate
  • 2006 Views
  • 2 replies
  • 1 kudos

LSM6DSOX: FIFO buffer not full when interrupt received.

Hey guys, I use a LSM6DSOX chip to collect data from both accelerometer and gyroscope. I used the integrated FIFO feature, with the following configurations:Accelerometer/gyroscope batch ODR = 104HzFIFO mode is Continuous modeInterrupt on INT2 is rou...

0693W00000Y9IyXQAV.png
MZhan.8 by Associate
  • 1240 Views
  • 0 replies
  • 0 kudos