MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The 210/109 combination allows for a register set to select 1666 Hz. If I run the device and do a read only, it may almost run at 1666 Hz, but if you do any real reads and analysis wanting the acceleration, time and frequency the device runs slower

I have about 10 of these devices on about 6 computers, so this problem is common, the device runs at about 1200 to 1400 Hz. The picture shows a temperature, frequency and FFT results plot for one device. The typical is about 1400 +- 50. I take and...

LIS2MDL single shot issues

When running the single shot with offset cancellation mode we will occasionally get the following measurements for the magnetometer:x = -1y = 0 z = -1 temp = -1 This causes issues for us as we are manually averaging the two single shot values togethe...

0693W00000Y7lE5QAJ.png
KPasm.1 by Associate
  • 1044 Views
  • 1 replies
  • 0 kudos

I am interested to use the device to determine the orientation of it in space using lis2dw12 only. As a test, I rotate the device 90 degrees each time over each one of the axes - Roll/Pitch and Yaw as presented in the attached figure.

I get the readings from ax,ay and az(plotted as well).Can the orientation of the lis2dw12 chip be derived from the DC levels? If so - how? What is the purpose of 6D orientation functionality and the accuracy of it?

SPiy.1 by Associate
  • 1209 Views
  • 0 replies
  • 0 kudos

FIFO timestamp (LSM6DSM)

Hi,i was trying to set up the pedometer and timestamp functionality for the FIFO.I was fallowing the instructions on page 102 (chapter 9.1) of the documentation for the setup (high timestamp resolution).It is working on a FIFO ODR of 104Hz. But if i ...

LHeit.1 by Associate II
  • 1999 Views
  • 1 replies
  • 0 kudos

Getting temperature from ISM330IS in AlgoBuilder

I have successfully built AlgoBuilder-based Firmware for my Target, including using some of the ISPU based examples from the x-cube-ispu GitHub:NUCLEO-L476RG + X-NUCLEO-IKS02A1 + ISM330ISWe are hoping to replace an old accelerometer and separate temp...

JLamb.3 by Associate II
  • 2461 Views
  • 3 replies
  • 0 kudos

MotionEC Update Rate

I'm using an LSM303AGR to create a compass using the MotionEC library for calculating quaternions.Since the ODR of the magnetometer inside the LSM303AGR is 20Hz while the ODR of the accelerometer is 25Hz with which frequency and with which data is it...

CSharpino by Associate III
  • 2179 Views
  • 3 replies
  • 0 kudos

Why i am not receiving a constant values?

Hello everyone!!!!I am using Motion_FX (9 axis) library in my application and receiving the values of Yaw, Pitch, Roll and Heading but these values, which i am receiving are not constant even if i kept the sensor in a fixed position values are varyin...

Anil3 by Associate III
  • 2349 Views
  • 3 replies
  • 0 kudos

MotionFX yaw problem

Hi, I use LSM9DS1 in my project. I also use MotionMC and MotionFX libraries to calibrate the magnetometer and fuse data respectively and I have a following problem regarding the yaw output. The roll and pitch work flawlesly but the yaw output reading...

Pajaka by Associate III
  • 1952 Views
  • 2 replies
  • 0 kudos