MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

we connected STM32F051 to ASM330 over SPI . The communication works only with Chip select line being toggled LOW as a GPIO line the SPI is not able to set Chip select Low . There is a 10K ohm Pull-Up resistor on the Chip Select Line . What is the suggeste

Hi ,We connected STM32F051 to ASM330 over SPI . The communication works only with Chip select line being toggled LOW as a GPIO line the SPI is not able to set Chip select Low . There is a 10K ohm Pull-Up resistor on the Chip Select Line . What is the...

ck.1 by Associate III
  • 1932 Views
  • 1 replies
  • 2 kudos

Resolved! ISM303DLC Library

Hi i am using ISM303DLC sensor could you please suggest me which library i have to integrate to get the Roll, Pitch and Heading.

Anil3 by Associate III
  • 1996 Views
  • 3 replies
  • 2 kudos

Is the LSM6DSL command set compatiple with LSM6DSM?

I have a custom PCB with a LSM6DSM accelerometer and it's being controlled with a nRF52 running Zephyr. The Zephyr RTOS sensor libraries only have LSM6DSL and LSM6DSO devicetrees. According to the initialzation functions it's communicating correctly,...

BKrug.1 by Associate II
  • 1408 Views
  • 1 replies
  • 0 kudos

Resolved! Conformal coating - LIS2DW12TR

Hi TeamWe are currently working on ST PN: LIS2DW12TR in our new project. Thus, I would like to check with ST whether this part is OK to be Conformal coated? The reason is, our PCB will need to be conformal coating after all the components are populat...

Resolved! SPI receive the same data every time (it's the register who_am_i)

Hi!I'm using the LaunchPad CC2642R1/CC2652R1 with the accelerometer LIS2DH and i tested the "who am i" (0x33) register to validate the protocol but when i tried read another register i had the same response that "who am i" (0x33) register. Could you ...

0693W00000Y8yEeQAJ.png
TVela.1 by Associate III
  • 2339 Views
  • 9 replies
  • 0 kudos