MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to configure S4S sensor synchronization in LSM6DSRX module

The iNEMO inertial module LSM6DSRX supports sensor synchronization S4S for Qualcomm. Sensor data sheet mentions following S4S registers without much detail.S4S_TPH_L (04h) Sensor synchronization time frame register - low byte (r/w)S4S_TPH_H (05h) S...

farid by Associate II
  • 2342 Views
  • 1 replies
  • 0 kudos

Resolved! LIS3DHTR Product Life cycle?

Hi,In the company where I work we are developing hardware and we are already evaluating the LIS3DH in order to put it in our hardware devices. However we have noticed that the LIS3DH is obsolete but there is the LIS3DHTR which is the same product but...

VGuer by Associate II
  • 6006 Views
  • 11 replies
  • 0 kudos

LIS2DH12TR- Not working on 2.9V and above voltages

Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...

Smalik by Associate II
  • 7893 Views
  • 22 replies
  • 0 kudos

Resolved! [STPM3x] Production date ?

Hi,I have a STPM33 on some of my PCB and I have issue with some of them when it gets too hot. The actual datasheet tells us that the operating temperature range is -40C to +105C but I've found an old one of October 2013, another of October 2014, anot...

carton by Associate II
  • 2090 Views
  • 3 replies
  • 0 kudos

Resolved! MEMS SMD device marking "SO"

Hi, can anybody tell me what partnumber this is. The chip is a LGA-14 package with the "SO" marking. It is probably an accelerometer.I aslo tried to read the 2d matrix code and it says: 781120R903QE

WVleu.1 by Associate II
  • 4004 Views
  • 4 replies
  • 0 kudos

Selecting a motion sensor

Hi,I am looking for a motion sensor with I2C that can work in the following way:Wake up from low powerStart monitoring acceleration and rotationStop monitoring (about 500ms later)Query most significant motion while monitoringGo back to sleepBasically...

Resolved! LPS22 Device ID

HiI try to read the WHO_AM_I register using SPI but I get 0xB3 instead of 0xB1. Is this correct?Regards

LMatt.5 by Associate
  • 1507 Views
  • 1 replies
  • 0 kudos

LSM6DSMTR Taking more power on VDDIO Pin

I am using LSM6DSMTR  with a coin cell battery. I have connected the IMU with NRF52810 using a SPI line. Attached the screenshot.When I am observing the power profiler, VDDIO is gradually taking current after the SPI communication (I have used a 100...

0693W00000Y9CiiQAF.png 0693W00000Y9CkKQAV.png
V.Jose by Associate II
  • 1897 Views
  • 2 replies
  • 1 kudos