MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DC bias from MEMS microphone using ADF on STM32U5

I have a MEMS microphone (IM72D128V01, using this eval kit) with PDM output connected to a STM32U5 NUCLEO board.It's connected to the ADF/Audo Digital Filter peripheral which I have configured to provide a 5th order CIC filter with a 32x decimation f...

DGran.3 by Associate II
  • 3640 Views
  • 3 replies
  • 0 kudos

Thermal response

One of the critical measurements for the analysis of bridges is the thermal response. The 201/109 combination has an average thermal response in the FFT of 1.5 milli-g - it is slightly frequency dependent, but ignoring that the standard deviation mea...

L3GD20 does not send the x y an z acceleration values

hello,I am using the L3GD20 to measure the angles, I have a 10 ms interrupt and in this interrupt service routine I read each time the 6 Output registers, I am configuring the gyro like this:GyroscopeDriver.TL3GD20_Reg_Struct.Who_Am_I = I_AM_L3GD20; ...

0693W00000aIUXFQA4.png 0693W00000aIUeBQAW.png

Simple procedures to sleep and wake-up lsm6dso

Hi, I'm trying to implement sleep and wake-up function in my project. I read the AN5192 Interrupt generation, but doesn't work. My project use nrf52832 with I2C and init my gyroscope/accelerometer following the procedure below: write_register(LSM6DS0...

LClad.1 by Associate II
  • 2073 Views
  • 1 replies
  • 0 kudos

How to change a network called in FP-AI-CTXAWARE1 package?

Hello, I recently bought the STEVAL-MKSBOX1V1 card (Sensortile.box). I would like to perform emotion recognition from speech through a convolutional network of my own creation. I downloaded the FP-AI-CTXAWARE1 package and opened the project on STM32 ...

FRana by Associate
  • 1712 Views
  • 1 replies
  • 0 kudos

LSM6DS3TR-C not generating new data

I'm using a ​LSM6DS3TR-C and polling the status register to determine when the gyro or accelerometer have produced a new value. This works fine for the most part however, if the sensor is moved quickly, it locks up and the new data sample bits in the...

ALees.2 by Associate
  • 2262 Views
  • 2 replies
  • 0 kudos

Is there more technical info on the ISPU available?

I would like to use the ISPU on the LSM6DSO16ISTR for signal processing of both the internal and a few external sensors. I'm having trouble finding any details on the ISPU itself. How about:Instruction set architecture Register fileBoot loaderClockin...

MFlam.1 by Associate
  • 1072 Views
  • 0 replies
  • 2 kudos