MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB gives inconsistent readings

Please refer this thread. I don't think that the sensor can get damaged in such short period of time. Is it possibly due to moisture? At times I get 1018hPa which is even higher than sea level pressure of 1013.5 hPaPls help.

DGand.2 by Associate
  • 1386 Views
  • 1 replies
  • 0 kudos

LIS3DH读�?�FIFO为空 LIS3DH reads FIFO as empty

设置 ODR400HZ�?范围 2g�?�?�用 FIFO 并�?置�?模�?。读�?��?个寄存器的�?置没有问题。数�?��? 5 毫秒读�?�一次,FIFO �? time_ src=0x20 读�?�一次。

jzhon.3 by Associate
  • 1230 Views
  • 1 replies
  • 0 kudos

SensorTile.box: Send data/text over Bluetooth to be displayed on PC.

Hi, I have created a machine learning model using STM32Cube IDE and would like to print out the results of the model on the PC using Bluetooth. I am using the SenorTile.box (STEVAL-MKSBOX1V1) with the SPBTLE-1S Bluetooth module.I am currently printin...

Bxy by Associate II
  • 1341 Views
  • 0 replies
  • 0 kudos

STEVAL-MKI109V3 and STEVAL-MKI197V1 IMU data rate to 6667Hz

Motherboard: STEVAL-MKI109V3 (STM32F401VETX)IMU board: STEVAL-MKI197V (LSM6DSOX)​Hello, I have ran into trouble setting the LSM6DSOX data rates of the XL and GY to 6667Hz in a custom STM32 project. The data is still fetched at a lower rate of around ...

vv.tl by Associate
  • 1793 Views
  • 2 replies
  • 0 kudos