2025-11-03 4:39 AM - last edited on 2025-11-03 11:59 AM by Issamos
Dear ST Support Team,
I’m currently trying to run the ST67W6X_CLI application (from the Wi-Fi ST67W6X CLI Wiki)
using the following setup:
Wi-Fi Expansion Board: X-NUCLEO-67W61M1
Host MCU Board: NUCLEO-F446RE
IDE: STM32CubeIDE (latest version)
Middleware: FreeRTOS (as provided in the ST67W6X_CLI example)
The project builds successfully and the firmware is programmed without errors, but at runtime, I encounter a HardFault_Handler.
The fault occurs inside the FreeRTOS queue management code, specifically during a call to xQueueReceive() in queue.c.
When the fault occurs, the debugger stops inside:
prvCopyDataFromQueue(pxQueue, pvBuffer);
and the corrupted member is:
pxQueue->uxItemSize
Observed value: 536871212 (0x2000412C) — which clearly points to an invalid or corrupted queue structure.
Call stack snapshot:
HardFault_Handler()
prvCopyDataFromQueue() at queue.c
xQueueReceive() at queue.c
spi_get_txbuf() at spi_iface.c
Please see the attached screenshot (from STM32CubeIDE) showing the variable states at the moment of the fault.
#### Welcome to ST67W6X CLI Application #####
build: 02:35:06 Nov 3 2025
--------------- Host info ---------------
Host FW Version: 1.1.0
[ERROR] [4000] [ST67W6XTask] (w61_at_common.c:375) sem_if_ready not received
[ERROR] [4000] [ST67W6XTask] (w61_at_sys.c:314) Could not init Modem handler
[ERROR] [4000] [ST67W6XTask] (main_app.c:791) [ERROR] in W6X_Init API
[ERROR] [4000] [ST67W6XTask] (w6x_sys.c:101) W61 Init failed
[ERROR] [4000] [ST67W6XTask] (main_app.c:291) failed to initialize ST67W6X Driver, 2
Application end
Note:
This output appears only during debugging. When the application is executed standalone (without debugger), no console output appears and initialization fails silently.
The project compiles and links successfully without any warnings or missing paths.
I have configured FreeRTOS parameters exactly as recommended in the CLI_App Example (including heap size and default task stack).
The configTOTAL_HEAP_SIZE and task stack sizes match the reference configuration.
some custom modifications were made to (fota.c).
The same application is confirmed to work on NUCLEO-U575ZI-Q, NUCLEO-H563ZI, and other officially supported boards.
So far, I have only flashed the host MCU (NUCLEO-F446RE) with the CLI example firmware.
I did not flash any binary to the ST67W6X module itself.
Could the issue (sem_if_ready not received and W61 Init failed) be caused by missing or outdated firmware on the Wi-Fi module?
Could this HardFault be due to memory alignment, DMA transfer, or structure packing differences on STM32F4 compared to the U5/H5 families?
Are there any additional adjustments to FreeRTOS memory or SPI interface required to make this demo compatible with F4 series MCUs?
Solved! Go to Solution.
2025-12-04 6:49 AM
The first thing to do is to update the binary in the ST67W611M1. You can do it directly from your PC if you have a UART dongle that connects the module's UART pins to your PC (while controlling CHIP_EN and BOOT pins as described here).
If this is not the case and the module's UART pins go to the NUCLEO-F446RE then you do indeed need to migrate the NCP_Loader project to this Nucleo board. Migration steps are generally the same as described in the wiki page. It should be easier to do as NCP_Loader is a simpler project. Note that you'd need to compile the project in the Bootloader configuration. Refer to 5.1 and 5.2 in this wiki page for more details.
2025-11-04 2:01 AM
Hello SelimMuhammed,
It appears that you have an ST67 module with an early binary that requires an update. This update is necessary regardless of the STM32 device you are using, including officially supported STM32 devices. Therefore, it is strange when you say that the application functions correctly on the NUCLEO-U575ZI-Q, NUCLEO-H563ZI, and other officially supported Nucleo boards.
Since you have a NUCLEO-U575ZI-Q board, connect it to the module and execute either CP_update_mission_profile_t01.bat or CP_update_mission_profile_t02.bat to update the module binary and load the CLI application binary. The choice between the t01 or t02 file depends on whether you want the LWIP to operate on the module or the host. After completing the update, verify that the CLI application is functioning correctly and that you can connect to a Wi-Fi network.
Once the module is updated, proceed to the NUCLEO-F446RE and check the status again.
Please share the results.
Best regards,
2025-11-04 6:03 AM
Thanks alot TarikAb
I really appreciate your reply
I would like to clarify something regarding this topic that when I said that the application functions correctly on the NUCLEO-U575ZI-Q, NUCLEO-H563ZI, and other officially supported Nucleo boards.
It was according to the wiki and documentation, not my experience so I didn't try to run CLI App on any of these boards.
Unfortunately, I don't have any of these Nucleo boards right now except the one that I have mentioned before (Nucleo-F446RE)
So, my question now: Could I flash the binary CP_update_mission_profile_t01.bat while I have this board (Nucleo-F446RE) as Host?
2025-11-04 6:21 AM
Hi again.
The short answer is yes but you need to go through some steps.
- Migrate NCP_Loader project to your NUCLEO-F446RE target just like you did with the CLI project and build it to generate the Bootloader.bin binary file. You could start from the U5 project which you can find under Projects\NUCLEO-U575ZI-Q\Utilities\NCP\NCP_Loader.
- Edit the .bat file so that it uses your Bootloader.bin and ST67W6X_CLI.bin files instead of the ones that were provided by the package.
- Run the .bat file
2025-11-05 4:03 AM
Hi again, TarikAb.
I would like to inform you that, I have migrated the CLI project according to the steps In the Wiki to build the project correctly although, I still have Runtime issues as I have mentioned in my post.
So, would you please recommend me a reference contains steps to migrate NCP_Loader project to my NUCLEO-F446RE target?
2025-12-04 6:49 AM
The first thing to do is to update the binary in the ST67W611M1. You can do it directly from your PC if you have a UART dongle that connects the module's UART pins to your PC (while controlling CHIP_EN and BOOT pins as described here).
If this is not the case and the module's UART pins go to the NUCLEO-F446RE then you do indeed need to migrate the NCP_Loader project to this Nucleo board. Migration steps are generally the same as described in the wiki page. It should be easier to do as NCP_Loader is a simpler project. Note that you'd need to compile the project in the Bootloader configuration. Refer to 5.1 and 5.2 in this wiki page for more details.
2026-03-22 7:50 AM
Hello SelimMuhammed,
I was facing the same hard fault on a F723 discovery board. My problem turned out to be a wrong pin assignment on the SPI interface connected to the ST67W611M1 . Fixing the pinout was all that was needed to get the Wifi modem running. I think this error is caused by a failure to communicate to the ST67W611M1 over SPI.