cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP - PQI stops RX timer at wrong channel

pelgrimo
Associate II

Greetings,

I'm working on a project where S2-LP scans multiple channels and receives a packet when a valid preamble is detected. For dwell time timing I'm using the RX timer. The timer is set to 2 milliseconds and is stopped whenever a valid preamble over certain signal level is detected to allow packet reception. Whenever the timer expires or a valid packet is received the next channel is selected (cycles from 1 to 10, then the cycle repeats) 

if(chSwitch)
{
  chSwitch = false;
  newChan = S2LPRadioGetChannel() + 1;
  if(newChan > 10)
  newChan = 1;
  subGHzSetChannel(newChan);
}

chSwitch flag is set in interrupt handler whenever the RX timer expires, or a valid packet is received.

Channel switching function:

void subGHzSetChannel(uint8_t chNum)
{
  S2LPCmdStrobeCommand(CMD_SABORT);
  S2LPRadioSetChannel(chNum);
  S2LPCmdStrobeCommand(CMD_RX);
}


Radio settings:

  • Base frequency: 915.5 MHz
  • Data rate: 10 kb/s
  • Frequency deviation: 20 kHz
  • Channel filter: 65 kHz
  • Channel spacing: 250 kHz
  • Modulation: 2-GFSK1
  • RX timer stop condition: CS AND PQI
  • PQI threshold = 4 transition (PQI_TH = 1)
  • RSSI threshold: -90 dBm

The receiver is a custom board. For transmitter I'm using STEVAL-FKI868V2.

The test: The receiver cycles through RX channels as described above. Transmitter transmits the following packet (transmit time = 51.2 ms) on channel 5 every 100 ms:

pelgrimo_1-1765266140748.png

The preamble length is set to cover dwell time of all ten channels + 1 dwell time + channel switching time.

The problem is that the timer is occasionally stopped at adjacent channels 3, 4, 6 and 7.

What happens then:

  • The timer doesn't expire
  • No valid packet is detected
  • The application is stuck until I set chSwitch flag manually o by a separate timeout
  • When I read LINK_QUALIF2 register (QPI value), it's indeed above QPI_TH.

I also tested transmission on different channels; the timer is always stopped at -2/+2 adjacent channels to the TX channel. The problem goes away when I increase PQI_TH value, but ideally, I don't want PQI_TH higher than 1, because it forces longer dwell time and longer preamble which affects the transmitter power consumption. Also, increasing PQI_TH feels like walkaround, because why would preamble be detected (RX timer stopped) on a wrong channel in the first place?

My question is, what would cause such a behavior and how to solve the issue? Has anyone encountered a similar behavior?

Thanks,

Marcin

 

1 REPLY 1
pelgrimo
Associate II

Update: Increasing PQI_TH seems the be the only way to fix the problem.
Update 2: During transmission on channel N, the noise floor is slightly elevated on adjacent channels N - 1 and N + 1. The noise was captured by the radio and falsely interpreted as valid preamble, so to avoid that I also increased RSSI_TH together with PQI_TH. The system works now, but it costs me some link budget unfortunately.