2025-11-05 12:24 AM - last edited on 2025-11-05 12:53 AM by Peter BENSCH
Hi there, I'm trying to figure out how to configure VD55G1 monochrome sensor to differential mode (e.g. disruptive mode, event mode) as branded in user manual. However, after going through https://github.com/STMicroelectronics/stm32-mw-camera, I have no clue. Could you help me with this? Thank you.
Solved! Go to Solution.
2025-11-05 12:35 PM
This is the frame subtraction function, which is also explained in Appendices B and C.
The difference between them is that Appendix B requires the host to process the subtraction, while Appendix C performs it on the sensor side. Both appendices also include sample code for your reference.
I have attached the sample code to enable the subtraction for you. For more details, please check the sample code in the appendices.
def enable_normal_internal_BG(self, exposure_mode):
"""
internal back ground subtraction with single context
"""
if self.m_bRunning:
iRet = self.m_dtccm.GrabHold(self.m_iDevID)
if iRet is None:
print("GrabHold in internal subtraction failed!")
if exposure_mode == 1:
self.set_exposure_mode(EXPOSURE_MODE_CTX0, 0x00)
else:
self.set_exposure_mode(EXPOSURE_MODE_CTX0, 0x02)
self.I2CWrite(VT_MODE_CTX0, 1) # VT_MODE = 1 : Subtraction on CTX0 , 0 : Normal Mode
self.I2CWrite_16(VT_SUB_WAIT_EXPOSURE_LINES, 0) # wait exposure lines between 2 sub-frames
self.I2CWrite_16(VT_SUB_WAIT_PIXELS, 0) # wait pixels between 2 sub-frames
self.I2CWrite_16(DARKCAL_PEDESTAL_CTX0, 0)
self.I2CWrite(GPIO_1_CTRL_CTX0, 2) # GPIO_1 = 2 (Strobe MODE)
if self.m_bRunning:
iRet = self.m_dtccm.GrabRestartWithSkip(0, 0, self.m_iDevID)
if iRet is None:
print("Restart frame in internal subtraction failed!")
time.sleep(0.5)
2025-11-05 11:34 AM
Hi,
For the event mode, please refer to Appendix G in the user manual. We call it the auto wake-up mode( AWU).
When the event occurs, the sensor will send a signal via the GPIO to the host. The host can then decide the next step, such as waking up the sensor to take a picture or activating other devices to perform certain actions.
I have also attached the sample register configuration for your reference below.
// -----------------------------------------------------------------
// This script has been automatically generated by GPSDK
//
// For better compatibility between platforms and V2Wreg
// You can force a transfer limit during generation:
// from gpsdk import config
// config.MAX_TRANSFER_SIZE = 64
// -----------------------------------------------------------------
$SCRIPT
SetBank(0x20);
// Set frequencies
WriteAutoIncrement(0x0220, 0x0, 0x1b, 0xb7, 0x0); // (val=12000000) / UI.SENSOR_SETTINGS.EXT_CLOCK.VALUE
WriteAutoIncrement(0x0224, 0x0, 0x8c, 0x86, 0x47); // (val=1200000000) / UI.SENSOR_SETTINGS.MIPI_DATA_RATE.VALUE
WriteAutoIncrement(0x0300, 0x40, 0x5); // (val=1344) / UI.STREAM_STATICS.LINE_LENGTH.VALUE
WriteAutoIncrement(0x0300, 0x68, 0x4); // (val=1128) / UI.STREAM_STATICS.LINE_LENGTH.VALUE
// => External clock = 12.00 MHz, Csi frequency = 1200.00 Mbps, Line time = 7.52 us
WriteAutoIncrement(0x0370, 0x0, 0x6); // (val=6) / UI.STREAM_STATICS.AWU_DETECTION_THRESHOLD.INTEGER
WriteAutoIncrement(0x036c, 0x42, 0x11, 0x0, 0x0); // (val=4418) / UI.STREAM_STATICS.AWU_CTRL
WriteAutoIncrement(0x0372, 0xbe, 0x1); // (val=446) / UI.STREAM_STATICS.EXPOSURE_USER_MAX_COARSE_INTEGRATION_LINES.VALUE
WriteAutoIncrement(0x036c, 0x42, 0x11, 0xa8, 0x8); // (val=2216) / UI.STREAM_STATICS.AWU_CTRL.FRAME_LENGTH_FOR_CONVERGENCE
WriteAutoIncrement(0x0312, 0x0); // (val=0) / UI.STREAM_STATICS.EXPOSURE_USE_CASES.ENABLE_MULTI_CONTEXT
WriteAutoIncrement(0x03e4, 0x10, 0x11); // (val=0) / UI.STREAM_STATICS.CONTEXT_NEXT_CONTEXT.CTX0
WriteAutoIncrement(0x03e4, 0x10, 0xf1); // (val=255) / UI.STREAM_STATICS.CONTEXT_NEXT_CONTEXT.CTX3
WriteAutoIncrement(0x03dc, 0x0, 0x0); // (val=0) / UI.STREAM_STATICS.CONTEXT_REPEAT_COUNT_CTX0.VALUE
WriteAutoIncrement(0x03e2, 0x0, 0x0); // (val=0) / UI.STREAM_STATICS.CONTEXT_REPEAT_COUNT_CTX3.VALUE
WriteAutoIncrement(0x0500, 0x0); // (val=0) / UI.STREAM_CTX0.EXPOSURE_MODE.MODE
WriteAutoIncrement(0x050c, 0xa8, 0x8, 0x0, 0x0); // (val=2216) / UI.STREAM_CTX0.FRAME_LENGTH.VALUE
WriteAutoIncrement(0x051d, 0x2); // (val=2) / UI.STREAM_CTX0.GPIO_0_CTRL.Mode
WriteAutoIncrement(0x051e, 0x5); // (val=5) / UI.STREAM_CTX0.GPIO_1_CTRL.Mode
WriteByte(0x0537, 0x00); // (val=0) / UI.STREAM_CTX0.MASK_FRAME_CTRL
WriteAutoIncrement(0x05fc, 0xe3, 0x67, 0x0, 0x0); // (val=26595) / UI.STREAM_CTX3.FRAME_LENGTH.VALUE
WriteAutoIncrement(0x060d, 0x2); // (val=2) / UI.STREAM_CTX3.GPIO_0_CTRL.Mode
WriteAutoIncrement(0x060e, 0xd); // (val=13) / UI.STREAM_CTX3.GPIO_1_CTRL.Mode
WriteByte(0x0627, 0x01); // (val=1) / UI.STREAM_CTX3.MASK_FRAME_CTRL
2025-11-05 11:43 AM
I guess I made it ambiguous. This is what I'm looking for.
2025-11-05 12:35 PM
This is the frame subtraction function, which is also explained in Appendices B and C.
The difference between them is that Appendix B requires the host to process the subtraction, while Appendix C performs it on the sensor side. Both appendices also include sample code for your reference.
I have attached the sample code to enable the subtraction for you. For more details, please check the sample code in the appendices.
def enable_normal_internal_BG(self, exposure_mode):
"""
internal back ground subtraction with single context
"""
if self.m_bRunning:
iRet = self.m_dtccm.GrabHold(self.m_iDevID)
if iRet is None:
print("GrabHold in internal subtraction failed!")
if exposure_mode == 1:
self.set_exposure_mode(EXPOSURE_MODE_CTX0, 0x00)
else:
self.set_exposure_mode(EXPOSURE_MODE_CTX0, 0x02)
self.I2CWrite(VT_MODE_CTX0, 1) # VT_MODE = 1 : Subtraction on CTX0 , 0 : Normal Mode
self.I2CWrite_16(VT_SUB_WAIT_EXPOSURE_LINES, 0) # wait exposure lines between 2 sub-frames
self.I2CWrite_16(VT_SUB_WAIT_PIXELS, 0) # wait pixels between 2 sub-frames
self.I2CWrite_16(DARKCAL_PEDESTAL_CTX0, 0)
self.I2CWrite(GPIO_1_CTRL_CTX0, 2) # GPIO_1 = 2 (Strobe MODE)
if self.m_bRunning:
iRet = self.m_dtccm.GrabRestartWithSkip(0, 0, self.m_iDevID)
if iRet is None:
print("Restart frame in internal subtraction failed!")
time.sleep(0.5)
2025-12-01 10:47 AM
Hi @ST-Chad
Thank you very much for your explanation "The difference between them is that Appendix B requires the host to process the subtraction, while Appendix C performs it on the sensor side. Both appendices also include sample code for your reference."
Will