cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with TOF050C-VL6180X time-of-flight (TOF) sensors

Jwinns
Associate

Maybe someone can help me. I bought five TOF050C-VL6180X time-of-flight (TOF) sensors, which also work with the Adafruit_VL6180X library, but they behave completely differently:

Two:
At a distance of 30 mm, the script shows: 0 mm
At a distance of less than 30 mm, the script shows: VL6180X_ERROR_RAWUFLOW "Raw reading underflow"

One:
At a distance of 20 mm, the script shows: 0 mm
At a distance of less than 20 mm, the script shows: VL6180X_ERROR_RAWUFLOW "Raw reading underflow"

The other two: The script shows approximately the correct distance, and you can also Get unlimited close without triggering the "raw reading underflow."

However, for my project, I need four sensors that are calibrated approximately the same. What can I do? Does anyone have any ideas?

1 REPLY 1
Anne BIGOT
ST Employee

Hello,

TOF050C-VL6180X time-of-flight (TOF) is not a ST reference.

Please contact the board maker to get support on this topic.

Thanks

 


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'