cancel
Showing results for 
Search instead for 
Did you mean: 

Drivers for VD56G3 Camera Sensor with STM32N6

Brenden_PLUS
Senior

Related posts

https://community.st.com/t5/imaging-sensors/integration-support-for-vd56g3-camera-sensor-with-stm32n6/m-p/822221#M5767

https://community.st.com/t5/imaging-sensors/drivers-for-st-brightsense-image-sensors-for-stm32n6-series-%CE%BCcs/td-p/757056

 

Setup 

* Camera - https://www.st.com/en/evaluation-tools/steval-56g3mai.html

* STM32N6570-DK

 

Question

I'm trying to find the drivers for the VD56G3 but i can't seem to find them.  The above posts say to go to this website

https://www.st.com/en/development-tools/stm32n6-ai.html#get-software

But when i go there its mostly about AI and the one thing about image capture goes to this which is just a binary blob?

https://github.com/STMicroelectronics/x-cube-n6-camera-capture

I do see this library

https://github.com/STMicroelectronics/STM32N6-GettingStarted-ImageClassification/tree/main/Middlewares/Camera_Middleware

 

If that is the driver how to i enable it in the IOC file?  I don't see it in the middleware and software packs. 

 

Secondary question 

* Is there a XThread version of this library.  Most of my app is XThread based.  

 

1 ACCEPTED SOLUTION

Accepted Solutions
Jean_Poire
ST Employee

Hi @Brenden_PLUS ,

You are correct the drivers are located there STM32N6-GettingStarted-ImageClassification/Middlewares/Camera_Middleware/sensors/vd6g at main · STMicroelectronics/STM32N6-GettingStarted-ImageClassification · GitHub.

This is the only version of the driver that we have for now and the middleware they are part of is not yet integrated inside cubeMx environment. You will have to add it manually to you project for now.

 

Best regards. 

Jean 

View solution in original post

2 REPLIES 2
Jean_Poire
ST Employee

Hi @Brenden_PLUS ,

You are correct the drivers are located there STM32N6-GettingStarted-ImageClassification/Middlewares/Camera_Middleware/sensors/vd6g at main · STMicroelectronics/STM32N6-GettingStarted-ImageClassification · GitHub.

This is the only version of the driver that we have for now and the middleware they are part of is not yet integrated inside cubeMx environment. You will have to add it manually to you project for now.

 

Best regards. 

Jean 

Hi Jean @Jean_Poire and Brendan @Brenden_PLUS ,

Thank you very much - we're also planning to use the 1.5 Mp VD66GY, VD56G3, VD16GZ or the planned 5 Mp VD5943 or VD1943 with the STM32N6x7 so it would be great to know when the drivers and middleware are integrated with STM32CubeMX and STM32CubeIDE :)

Will