Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can XSHUT & GPIO pins in a multiple VL53L0X configuration handle 5V when interfaced to a 5V Microcontroller like Arduino Mega?

I see from this GY530 schematic that the module has level converters for the I2C lines, but not for GPIO & XSHUT lines. When using a 5V micro-controller like an Arduino UNO or MEGA to run multiple VL53L0Xs using XSHUT to configure addresses, will dr...

FPayn.1 by Associate III
  • 3768 Views
  • 3 replies
  • 0 kudos

Difference between Long Distance Mode and Short DM - VL53L1X

What is the difference betwen Long DM and Short DM in terms of principle of operation?For example in ULD API for Short Distance Mode these registers are used:status = VL53L1_WrByte(dev, PHASECAL_CONFIG__TIMEOUT_MACROP, 0x14); status = VL53L1_WrByte(d...

rothosen by Associate
  • 1306 Views
  • 1 replies
  • 0 kudos

I can't use VL53L1x sensor from other micro controller.Because there is no related document(s).Please help me about its registers init sequence and reading sequence to measure distance. Regards.

I can use this senser only together ST micro controller.Also its freeware APIs not enough for this purpose.I think ST must provide neccessary support about this subject without need anycustomer feed back.( Because VL53L1X is belong you )Regards.

OOCAK.1 by Associate
  • 1145 Views
  • 1 replies
  • 0 kudos

Why am I getting VL53L0X Error: -6?

I have a single 'known good' VL53L0X hooked up to an Arduino Mega 2560 through a bidirectional level shifter. When I attempt to initialize it I get the following output:Opening port Port open Arduino Hex VL53L0X Demo In Adafruit_VL53L0X::begin(29,1,...

FPayn.1 by Associate III
  • 2398 Views
  • 2 replies
  • 0 kudos

Resolved! Calibration

Hello I am new in the field of Tof sensors I would like to know how you proceed to carry out your calibrations? are there any software manipulations to perform? I read in a conversation in which you spoke about function and variable Xtalk .. If so, p...

MSAMB.1 by Associate III
  • 1737 Views
  • 2 replies
  • 0 kudos

How to troubleshoot I2C bus sensor response problem?

I have a project where I am attempting to use six ST Microelectronics VL53L0X Time-of-Flight (ToF) sensors grouped into two 3-element arrays for position/orientation sensing on an autonomous wall-following robot. I originally had both arrays installe...

FPayn.1 by Associate III
  • 3491 Views
  • 5 replies
  • 0 kudos

Sensor test with evaluation cards

I am currently in the process of doing a study on the VL53L0X, VL53L1X, VL6180X, VL6180 sensor I carry out distance and air gap tests on each sensor, the goal is to choose the ideal sensor to carry out proximity detection for the access control. So I...

MSAMB.1 by Associate III
  • 1124 Views
  • 1 replies
  • 0 kudos