Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L0X returning "0" for SignalRateRtnMegaCps?

Hi,I am running into a problem where the VL53L0x will return "0" for its SignalRateRtnMegaCps value for certain range measurements. Some sensors I have it does this an overwhelming amount of the time. Some sensors I only see this periodically.I use t...

MFord.1 by Associate III
  • 1796 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX not generating code correctly

I am trying to explore X-CUBE-TOF1 and I have several VL53L3CX breakout boards. I'm using the latest CubeMX and IDE (6.3.0 and 1.7, respectively) and therefor downloaded both the 2.0.0 and 1.0.0 X-CUBE-TOF1 cube modules.I've selected the following ...

0693W00000D2CIIQA3.png 0693W00000D2CINQA3.png 0693W00000D2CISQA3.png 0693W00000D2CIhQAN.png

VL53L1 Ambient light measurement

Hi all,I'm working on a project where I need to analyze the raw histograms from the VL53L1 sensor. For my analysis to work I need to subtract the ambient light from the histograms.I get the histogram data using VL53L1_GetAdditionalData(), and I can s...

PZagu.1 by Associate
  • 2766 Views
  • 3 replies
  • 0 kudos

I am trying to wire the VL53L1X-SATEL breakout board to a microcontroller (ESP32) yet the pinout is not clearly defined (even in the datasheet). Is VDD supposed to be the voltage input (between 2.8V and 5V) ?

If the VDD pin on the left (breakable) part of the breakout board actually is the input voltage, then there is a problem, for the voltage drops and it even causes a brownout.

CLE.11 by Associate
  • 1637 Views
  • 1 replies
  • 0 kudos

Multiple sensors generate interference between each other

Hi ST team and community !I'm here because i have some troubles on the VL53L1X.I use the following library available on GitHub : openmv/vl53l1x.py at master · openmv/openmv · GitHub.I deployed several VL53L1Xs around the mobile robot, hoping to get t...

Zjun.3 by Associate
  • 1999 Views
  • 1 replies
  • 0 kudos