Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X detect wrong with black object

Hi,I'm building a project that uses 20 VL53L1x sensors to detect any people or objects that go in the danger zone of a machine.The sensor will detect any objects or people below 2 meters distance. We set up the sensor 30cm above the ground.The measur...

HHo.4 by Associate
  • 1674 Views
  • 1 replies
  • 0 kudos

Resolved! Allowable vibration levels for time of flight sensors

Has ST done any research into the level of vibration these sensors can safely withstand? I'd like to use these on an application which experiences intermittently high vibration (up to 15m/s^2, mostly parallel to the sensor measurement direction). Acc...

JStra.4 by Associate II
  • 1370 Views
  • 1 replies
  • 0 kudos

Cannot load Firmware to VL53L5CX

With the following code the VL53L5CX should get it's firmware uploaded. "   /* Download FW into VL53L5 */   status |= WrByte(&(p_dev->platform), 0x7fff, 0x09);   status |= WrMulti(&(p_dev->platform),0,           (uint8_t*)&VL53L5CX_FIRMWARE[0],0x8000...

LCord.1 by Associate III
  • 2500 Views
  • 4 replies
  • 0 kudos

VL53L0X Restore Factory Default Calibration

Hello, is there a way (after applying a calibration such as offset calibration or crosstalk calibration) to return the sensor back to the default calibration that was performed at ST? If so, which I2C commands would perform this job?

Rkoons17 by Associate II
  • 3012 Views
  • 4 replies
  • 0 kudos

Resolved! Detection thresholds confusion

A couple of questions.First there seems to be some conflicting comments. In the vl53l5cx_plugin_detection_thresholds.h file there is the following statement in regard to the mathematical operators for multiple checkers. "Please note that the first c...

BBald.1 by Associate II
  • 2391 Views
  • 4 replies
  • 0 kudos