Hello, I'm running ubuntu 24.04 and running STM32CubeMonUCPD with "jara -jar SetupSTM32CubeMonitor-UCPD.jar" fails with error Command line arguments: SEVERE: java.lang.ArrayIndexOutO...
Hi I have the cube monitor plugged in , and running the cube monitor power application. I had it working on my old computer (Windows 10) , but had to install the USB driver of ST web site. Si...
Hi, STM32CubeMonitor-UCPD sometimes displays RDOs like this: Where does the number MaximumOperatingCurrent come form? Since the RDO is defined as: typedef struct
{
uint32_t MaxOperatin...
Hallo, I am saving the log files of the chart in the CUBEMonitor software. I read certain values from the MCU through Cube Monitor and save them as .CSV. However I've noticed that the first ...
Dear All, I want to use STM32CubeMonitor to monitor 64-bit variables, such as int64_t or uint64_t. However, it seems that 64-bit variables cannot be selected from the variable ...
Hello, I am using STM32-U585I-IOT02A board. I have initialized USB-C SINK TCPP project with fixed 9V settings. On STM32CubeMonUCPD, 'ibus(mA)' value is always zero when connected BMS board shows cha...
Hello, Would it be possible to have the correspondence of the JSON type according to the type of variable we put? Please I've been able to identify a few such as : type 1 -> uint8_t type 3...
Hello, I am using the latest version of STM32 Monitor with STLink V3 probes, and everything is working correctly. My only issue is the refresh rate of the STLink probe status on STM32CubeMonitor, w...