I just bought 10 pcs of LDL1117S33R which i plan to use them to power 3.3V modules form a 4V regulated source. According to the data sheet the typical dropout is 350mV and max is 600mV @1....
I'm using the L6981C33DR bug converter to convert 24V (from an SDR-120-24 power supply) down to 3.3V. However, I've had instances where the regulator overheats and "exploaded". The circuit only need...
Where can I find the source code for the firmware on the STEVAL-WLC38RX and STEVAL-WBC86TX boards? I'd like to start there and make some modifications. Thanks.
Hello, Recently, I purchased the STEVAL-SWLC38RXA and STEVAL-SWBC86TXA eval boards from Mouser. After some digging, I found the GUI and downloaded the STSW-WPSTUDIO v2.7.2. When I connect...
I get an error message when I try to connect with the STEVAL-WLC38RX evaluation board using STSW-WPSTUDIO. I am using v2.7.2 of WP Studio. See error message attached.
I'm working on a low-power design and planning to use a STLQ020. The datasheet doesn't mention the need for a protection diode, nor does it mention that there is one integrated.. Is there an integ...
Hello, Could you please direct me to a complete reference design schematic? The one provided in the datasheet appears incomplete, and many of the forum links on this topic seem to be inactive. Your...
Hey, probably a dumb question, but I couldn’t find it in the datasheet. Can each pin of the VNQ9025AJ handle 30A, or is that the rating for the smart switch as a whole with a limit on each pin? Hones...