Hi, I have connected a MAX-M10M module to an STM32H7 MCU ( it's custom board) by UART port. I am able to send data to GPS module and also receive config data of it but not able to receiv...
I have a question regarding the use of the STSAFE-A110. Currently, the default I2C address of the STSAFE-A110 is set to 0x20. It is possible to change this address? If it is possible, could you ple...
Hello everybody, I am currently programming on a STM32G0 for a screen with the st7567 driver. I created a function to display a text. When indicating the information on the font I have a warning f...
Hello, I am currently designing a battery-powered device that incorporates the STUSB4500. I have a question regarding the I²C pins: specifically, whether it is safe for these pins to be pulled up (v...
Hey, I am working on Xbee with stm32, and I am getting a big problem while connection.
I am using two Xbee's one is configured as a standard router which is connected to UART1 of the ...
Hello, this is the ECMF4-40A100N10(MIPI DSI ESD protection). I want to implement it in my design and I was wondering if it matters to connect your positive differential pair signals to D1+ and D...
HI ST teams,
I 've purchased STPM4RasPIV21 to test our SPI master device. I'v observed this TPM IC uses wait state when communication. Please help share behavior model(verilog) for SPI master simul...
I would like to inquire about the thermal resistance (θJA) of this specific part. Could you kindly provide the θJA value or direct me to the relevant technical documentation? M95128-DFCS6TP