What is the type of internal (mechanical) structure of LSM6DSO32 gyro sensor? (a photo of the internal structure would be beneficial). The reviewer asked us about this during the review process, and ...
I am conducting research on robot control, and to handle data obtained from the LSM6DS3H embedded in the robot, I want to understand how acceleration and angular velocity are measured. Specifically, ...
Hello. I wrote the following code to use the LSM9DS1 sensor with the STM32 WB55RG board. The current issue is that when I set the gyro to 0x18 and the accel to 0x28, as specified in the sensor datash...
We have a STEVAL-MKI224V1 kit, which should be equipped with a LPS22DF. I have tried to use the static (I2C) address of the sensor, and after much time, I discovered it is (depending on the state of ...
Hi, We've been working on a project using v1.3.1 of MEMS Studio, but I've had to use a new laptop and it doesn't have this installed. Unfortunately, when I go to the downloads page I can only see v1...
Hello, I'm designing a custom board with a LIS2DW12 accelerometer for motion detection. I want to use INT1 to send a signal to the MCU when it detects movement, which should wake up the whole system...
I BOUGHT STEVAL- MKBOX PRO AND AM THINKING OF USING IT. I have a wireless function, but please tell me the status of technical conformity approval for use in Japan. There was no conformity mark on ...
Hi, I am working on a custom ISPU code for LSM6DSO16IS and I want to generate interrupts on INT1 and INT2. I checked all the examples in x-cube-ispu/Ispu/ism330is_lsm6dso16is at main · STMicroelectr...
I would like to change the state of the INT_DRDY of LPS22DF. I have tried to change the value of INT_H_L bit in register CTRL_REG3 (12h), but it has no (immediate) effect. Is it necessary to activate...