Hello, I'm working with a graphics output on an STM32H750-based board. My bitmap resources are stored in SQPI, and the frame buffers (double buffering) are in external SDRAM. The external SDRAM se...
How to use TouchGFX with an MCU and a TFT that isn't listed in TouchGFX ? My board is a Nucleo-STM32H753ZI and the TFT is an ILI9486 420 x 380. Thanks.
I have just started using TouchGFX on an Stm32H7A3ZIQ Nucleo board. I managed to setup the LTDC correctly and am able to change the color of the screen, which makes me assume that the LTDC is setup c...
Hi all, For my GUI I need several circle and box progress widgets in different sizes that have a transparent background, e.g. only showing the actual progress "line" and nothing else. So far I achie...
Hi, I’d like to use the vectorized version of a font (bebas-neue-regular.ttf), but the glyphs don’t quite match the original shape. Why is that, and how can I fix it? Could it have...
I try implement 1424x280 DSI panel and it work, but transition on single buffer have trouble. I start with simple fadeout and attached video show result. Try off DCACHE ICACHE DMA2D GPU2D, no big di...
i want to use touchgfx make UI's for board STM32H750VB with display 2.8inch 240*320 ST7789 driver. > In touchgfx designer i have choose STM32H750 DK for my board ? is there any anothe...
I use the platform of STM32H747 to play a video with AVI format, if the frame width*height=568*320, touchGFX can't play this and skip this function, which type of resolution can be used for tou...
Hello, we previously used the STM32U5G9J-DK2 discovery kit with FreeRTOS and TouchGFX (with hardware-accelerated Vector Font Rendering, etc) successfully. Now we are trying to bring up a custo...
Hello All, I need to change the touch GFX project name MyApplication_747I to something else, I am trying to change it from config but touch gfx is not allowing it to change. I tried...