Hello, I am currently reviewing the S2-LP transceiver for high-bitrate/long-range communication in the 915MHz band. To achieve that, I want to interface an S2-LP with a Skyworks SE2435L front-end, a...
Hi, I have some questions regarding the ST60x parts Do you have a bulk quantity price estimate for the ST60A2 and ST60A3H1 parts? Are there recommendations for transmitting parallel...
Hi, Some time ago I wrote a software with some changes from this library and successfully tested it with the STEVAL-FKI868V1 board and a ST board (STM32F779 EVAL). Now I made my own hardware with a...
Hello,
We are looking to develop an efficient battery-powered device and I wanted to know the active and the standby power consumption figure at 1.8V for the ST4SI2M0020TPIFW eSIM module. Ther...
Hi, I am trying to write the IQ data to the SD card (i.e., write the received CTE pkt to the SD card). However, I found that Bluenrg-332ac has a cortex M0 core, which may not be able to drive an SD ...
Hi, I am currently working with the documentation of TCPP01-M12. I have find some small mistake in the table of recommended capacitor C3. The part codes are switched. Also it seems that the GRM188.....
Hello, I hope you are well. I have a question about the certification of the “Programmable Bluetooth® Low Energy wireless SoC” from the “BlueNRG-LP” family: are they BQB certified? Thanks in advan...
Hi. Please can someone tell me whether Part No: M24LR04E-RMN6T/2 (RFID Transponder) is able to communicate with MiFare Desfire ? Application will be a custom designed PCB to be used as part of...
Does anyone have any details on register settings to get the S2-LP running from XIN rather that a crystal? The documentation is a bit thin in this area.
I am trying to get 12V at the output of STKNX buck converter, but I am not getting it and the STKNX dead. The RFB1 that I am using is 33K Ohm and the RFB2 is 3k Ohm, with these resistors the Vout wo...