While researching the GNSS module for my project, I got somewhat confused about the power connection of the LIV4F module due to inconsistent information in the manuals. The general recommendation is ...
Hi, as the title said, I am having the hard time communicating with X-NUCLEO-GNSS1A1 The GNSS module is communicate via USART (can't communicate via I2C, but this is the other problem) the code...
Hi, I have tons of question about the command $PSTMSETPAR and some related command: First of all, I would like to change the NMEA Baudrate to 38400, as the software manual said, I should transfer...
Hi, I can't get the correct fix rate for x-nucleo-gnss1a1 Using following command: $PSTMSETPAR,1303,0.1,0 $PSTMSAVEPAR $PSTMSRR what I expected is update rate 10Hz, i.e., the timestamp is ...
Hi, I would like to know the maximum velocity that the TESEO LIV3F chip can still having a stable update rate. I'm currently doing localization using TESEO LIV3F, and it update the position very s...
I have the "TeseoSuitePro_6_1_3" suite. It comes with installed bin files for STA8089GAT. After I flash the firmware that arrives with the tool I get the tool to start , it sees the GPS satellites wi...
I do not understand how to properly boot from SPI as it contradicts the BOOT table in the guide document for the STA8089GAT pins on page 22 (“STA8089GA-Pin-by-Pin-guideline.pdf�?). To boot from SPI ...
In the STA8089GA circuit guideline document it is noted throughout the document several times to refer to a special application note about standby mode specifically. It is actually referencing to s...
Hi, I'm currently playing with the X-NUCLEO-GNSS1A1 kit and I have two questions: -If I only configure Galileo the messages are still GPGLL and I do not get GAGLL for Galileo and I do not know wh...