Hello, i'm currently working on the stm32mp135f-dk with the kirkstone yocto version for layers provided by st. I'm trying to double all fs partitions (rootfs bootfs and userfs) to implement a softwar...
Hi there, I am working on an OSD32MP157F custom board inspired by STM32MP157F-DK and Octavo Red boards. The pinout is very similar to the stm32mp157f-dk with the main difference that th...
I would like to use the Murata Wi-Fi/BT combo module 2BC on STM32MP1. Is it possible? If it is possible, I would like to know how to integrate 2BC on STM32MP1. I understand following. - M...
Hi ST Community, I am trying to flash a eMMC with STM32CubeProgrammer, in a STM32MP157F custom board. I am using a GPT partition file and a img. I can see the system is creating partitions and flas...
I'm attempting to upgrade from ecosystem v2 to v4 and I've run into an issue where the USB OTG port no longer enumerates at boot time. Specifically, I no longer see any messages in dmesg regarding th...
We are using developBoard by Emcraft with STM32MP157A. Emcraft release board with Openstlinux 4.14. If I want change devicetree of STM32MP1 i need use STM32CubeMX to export new devicetree. If i g...
Hi there, I have a custom board (with eMMC) that freezes in the middle of kernel loading: I am under the impression it is related with the rootfs.ext4, becuase it does not try the loading, but ...
I am trying to migrate from ecosystem 4.1.0 to 5.0.0 however after getting all the device trees to compile and build plus a new image I am encountering a Panic in optee. The problem is that it just s...