Hello, We propose using Teseo-LIV3FL to design a new product. This part is selected because it supports Differential GPS (SBAS) and Real-time AGNSS. Please let us know if LIV3FL supports NA...
Hello,
I am currently working with the NUCLEO GNSS2A1 extension on the NUCLEO-L010RB demonstration board, and I am trying to retrieve data from the gyroscope and accelerometer.
Acc...
Hi, I bought an EVB-LIV4F to evaluate LIV4F and I have sent two emails to st-teseo-suite-support@st.com to request activation code. Unfortunately, I haven't received any response. Is ...
Hi, We're attempting to update the LIV4F firmware via the UART interface from an embedded device, however, we're unable to replicate the steps documented in UM3009. Our code works up until ...
Hello I need to use full featured Teseo-Suite. Sending letters to st-teseo-suite-support@st.com remain unanswered. How could I obtain a full version of Teseo-Suite? Thanks
Hi, The BOM and almost all pictures of X-STM32MP-GNSS2 include a Taoglas antenna. Could you verify if an antenna is actually included or not, if I order an X-STM32MP-GNSS2?
Hello, I'm using a Teseo III module from Lantronix. When connected up, I can see NMEA sentences over UART, at 9600 baud. I have a few questions. I'm not a GPS expert, and unfortunately, the Teseo I...
What is the actual backup input supply voltage range for Teseo LIV4F receivers? Datasheet says that it is 3-3.63V which is really high and doesn't make sense to add any Lithium battery as a backup su...
Hi, Due to the limitation of height in our product, modules won't be suitable. I am currently considering STA8089FG. Could you send me the application note/reference design for this chip? Thanks.
Hi.. I have soldered a Teseo-LIV3 on a PCB with acces to power and RX/TX and nothing more. I read the NMEA strings, but no satellite data is present. Is it correct understood that Teseo-LIV3 ca...