STM32 MPUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Peripheral example for STM32MP135f-DK?

I am familiar with the STM32 MCU:s and now I try to learn some around the Linux MPU:s.I am looking for a simple pheripheral application example on how to control e.g some GPIO:s from inside Linux using the STM32CubeMX and STM32CubeIDE.Any hints?Thank...

Resolved! Help needed in configuring I2S supply voltage

Hi,Are there any references for configuring the I2S supply voltages in device trees for STM32MP135-DK.From the I2S module currently we are getting the output level as 5V, is that expected or is there any way to change that from 5V to 3.3V.

Resolved! STM32MP133 OTP Alternate QSPI Boot

Hello, In order to use the non-default QSPI boot locations, my understanding is port0-port3, 4 signals need to be defined in OTP words 3, 5, and 6 based on a similar question about SDMMC1 discussed here:https://community.st.com/t5/stm32-mpu-products/...

Jasper by Associate II
  • 883 Views
  • 4 replies
  • 0 kudos

stm32mp135 - pcm5102a - sai1a

Hello,I try to connect a popular Arduino board PCM5102a with my board which is base on STM32MP135.I read some documentation from the linkhttps://wiki.st.com/stm32mpu/wiki/ALSA_overviewhttps://wiki.st.com/stm32mpu/wiki/Soundcard_configurationhttps://w...

MWoo2_0-1688975337399.jpeg
MWoło.2 by Senior II
  • 1534 Views
  • 11 replies
  • 1 kudos

Resolved! S24_LE support on I2S of STM32MP1 line

Hi,what's the state of the S24_LE format support on the STM32MP1 line of boards? It seems that S16_LE and S32_LE formats are supported on the I2S dai, however S24_LE is rather unavailable. Is there a way to somehow enable it (maybe through Cube MX) o...

AJank.2 by Associate III
  • 613 Views
  • 2 replies
  • 1 kudos

Resolved! stm32mp135 PA10 as tim1 ch3 pwm

Hi,I have a problem with the configuration of PA10 of stm32mp135 to work as pwm of TIM1_CH3. I also make an experiment to disable completely timer and PWM and I also can't control this pin using gpioset. In the documentation I saw that this pin is de...

MWoło.2 by Senior II
  • 763 Views
  • 7 replies
  • 0 kudos