STM32 MPUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Failsafe FIP update with PSA_FWU_SUPPORT

Hi,i'm implementing our field-update using the A/B mechanism for FIP image.Would like to use the Update Client described on the page as a template:https://wiki.st.com/stm32mpu/wiki/Secure_Firmware_Update#Update_ClientBut no idea where to find it. I d...

SimK by Associate II
  • 350 Views
  • 3 replies
  • 0 kudos

STM32MP133CAF3 gpio pins configuration in the dts

Hi Team, I am new to STM32MP133CAF3 processor. I want to configure two gpio's as outputs in my Device tree source file. My pin numbers- > PE5  -> high & output_1-> PB0    -> high & output_2 These two pins I want to configure it.  Could you please hel...

Resolved! STPM4RasPI for STM32MP135F-DK - SPI timeout error

Hi, I would like to integrate the STPM4RasPI with MP135F-dk. After following the https://wiki.st.com/stm32mpu/wiki/STPM4RasPI_expansion_board tutorial, I am receiving an error. Driver is enabled:STPM4RasPI module is properly attached. Do you have any...

jschneider_1-1701174477269.png jschneider_0-1701175073672.png

Resolved! Double partitions to implement A/B update mechanism

Hello, i'm currently working on the stm32mp135f-dk with the kirkstone yocto version for layers provided by st. I'm trying to double all fs partitions (rootfs bootfs and userfs) to implement a software update mechanism with an active set of partitions...

retroll by Associate II
  • 1606 Views
  • 6 replies
  • 2 kudos

Resolved! Support for Murata 2BC CYW4373 chipset

I would like to use the Murata Wi-Fi/BT combo module 2BC on STM32MP1.Is it possible?If it is possible, I would like to know how to integrate 2BC on STM32MP1. I understand following.- Murata 1DX are mounted on STM32MP1 evaluation board.- Murata has th...