STM32 MPUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP135 - Baremetal - Ethernet2

Hello, I would like to integrate ethernet2 in my bare-metal project. I am aware that not only eth2 pins have to be properly configured, but also a 10th pin of MCP IO expander. However, the eth2 seems to be disabled after all. I am doing the same conf...

RTC Clock Source Selecton Issue - STM32MP135F

Hi,I'm having an issue with RTC module. getting an error due to no clock source is connected to rtc_ck:[ 3.645423] stm32_rtc 5c004000.rtc: rtc_ck is slow[ 3.749902] stm32_rtc 5c004000.rtc: Can't enter in init mode. Prescaler config failed.[ 3.756489]...

Resolved! stm32mp135 yocto build process

 i have download prebuild image en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gzit working fine on my stm32mp135f-dk EVK. i want to add docker in it so need the build process of yocto image.Kindly guide me how to do it.