STM32CubeMX (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157A, enable USART2 through ST-LINK

Hi,   I have a STM32MP157A-EV1 board. I'm running it in the engineering boot mode and programming the Cortex-M4 directly through the STM32CubeIDE. At the moment, I do not use the Cortex-A7.   I would like to enable USART2 and use it through the ST-LI...

0693W00000VOTVUQA5.png 0693W00000VOTVjQAP.png
Fnx_QT by Associate III
  • 474 Views
  • 4 replies
  • 0 kudos

Resolved! EXTI configuration in STM32CubeMx for STM32MP157F-DK2

I am having difficulties activating the EXTI interrupt for a pin in the M4 NVIC.   What I did: Opened STM32CubeMX,selected the board STM32MP157F-DK2,opted to configure all peripherals in their default stateActivate SPI5 in the M4 domain, incl. DMA do...

SFuch.1 by Associate III
  • 316 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to find STM32MP157D-DK1 board definition

Hi there!   I just purchased an STM32MP157D-DK1 discovery board, and noticed that in STM32CubeIDE there are no definition files for this model, only a subset of the other MP1 discovery boards (but curiously not all of them).   Is this product unsuppo...

etheory by Senior
  • 456 Views
  • 5 replies
  • 0 kudos

STMCubeMX device tree output for I2C5 on STM32MP157A-EV1

I'm attempting to activate I2C5 on I2C_EXT connector CN13 on the board. Prior instructions were to generate device tree code in STMCubeMX. Done that, but something looks weird. All HW documentation and EV1 user documentation indicates that I2C5 is ph...

ThePUP by Associate III
  • 323 Views
  • 2 replies
  • 0 kudos